Mouser and Microchip Present Embedded IoT Made Easy Webinar

Discover scalable and system-wide approach to creating smart, connected and secure IoT applications with Microchip Technology
För omedelbar lansering

Anslut till oss


August 23, 2021Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, has teamed up with Microchip Technology to bring the engineering community a brand new webinar. The Embedded IoT Design Made Easy webinar will detail the ease of developing a smart, connected and secure Internet of Things (IoT) application using Microchip Technology’s wide portfolio of products. The free live webinar will occur at 11 a.m. Central European Summer Time (CEST) on Tuesday, September 7, 2021.

The Embedded IoT Design Made Easy webinar will explore a range of solutions for how to efficiently design smart and secure IoT solutions using products like the PIC32 WFI32E Curiosity Board. With advanced features that include pre-provisioning for cloud platforms such as Amazon AWS, Microsoft Azure and Google Cloud, Microchip is also supporting easier on-boarding and off-boarding. The webinar will draw on Microchip’s total system solution comprising microcontrollers, microprocessors, FPGAs, RF modules, analogue, timing and power.

Smart connected devices are now getting even smarter, thanks to artificial intelligence (AI) and machine learning. These enabling technologies are moving closer to the edge and can now be more easily embedded into the most resource-constrained IoT endpoints. The webinar will explain how to securely access these important technological developments. The Microchip Technology solutions covered in the webinar include the SAM-IoT WG development board, which features the Arm® Cortex®-M0+ based SAMD21G18, the ATECC608A CryptoAuthentication™ secure element IC and the fully certified ATWINC1510 Wi-Fi® network controller.

The webinar will also cover fast prototyping using Microchip’s latest IoT-focused development kits, which support over 1,000 Mikroe Click boards. Attendees will learn how quick and simple it can be to get to a proof-of-concept stage, even when using AI and machine learning, by leveraging the power of Microchip’s advanced development environment.

IoT is synonymous with connectivity. As the popularity of low-power wide-area networking (LPWAN) grows, it will support more devices over longer distances. This webinar will explore the LoRa® SAM R34 Xplained Pro evaluation kit, an LPWAN IoT-enabled board, based on a SiP using an Arm Cortex-M0+ microcontroller, offering system power as low as 790 nA.  Local wireless connectivity is increasingly provided using Bluetooth® Low Energy, so attendees will also learn about the evaluation board using RN4870 Bluetooth Low Energy module, with integrated transceiver, RF amplifier and power management unit.

Delivering the webinar are Johan Pauvert, Microchip EMEA Wireless Marketing Manager, and Markus Austermayer, Microchip EU Sales Leader IoT Ecosystem, who offer more than 40 years of industry experience between them.

To learn more and to reserve attendance at the webinar for free, visit https://emea.info.mouser.com/embedded-iot-design.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För pressförfrågningar, kontakta:
Janice Fenton
Direktör för B2B-kundansvar med ansvar för originalitetsverifiering
+44 (0) 7984 077330
För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833