Melexis MLX90830 Triphibian MEMS Sensor, Now at Mouser Electronics, Delivers Reliable Pressure Detection in Harsh Environments
March 6, 2024 – Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the MLX90830 Triphibian™ MEMS pressure sensor from Melexis. With a cantilever design, the MLX90830 measures gas and liquid pressure in diverse environments with high precision and reliability. The sensor can be integrated as a standalone device or embedded in expansion valves, e-compressors, or pumps in electric vehicle thermal management systems. The MLX90830 IC is also a suitable choice for HVAC-R applications.
The Melexis MLX90830 sensor, now available at Mouser, is the first product to feature patented Triphibian technology. The advanced pressure sensor offers consistent performance and durability in all the conditions an electric vehicle is likely to experience. The sensor operates in temperatures ranging from -40°C to 150°C, measuring gas and liquid pressures from 2 to 70 bar while also surviving frozen states. The ability to measure gaseous and liquid states and survive solid (frozen) states means that the sensor can operate under all possible conditions. The factory-calibrated Melexis MLX90830 sensor IC delivers highly accurate measurements directly out of the box.
The device combines electronics and the sensor into a standard SO16-sized IC package. The patented sensing component is a piezo-resistive element configured as a Wheatstone bridge. The bridge output is amplified and sent through an analog-to-digital conversion stage. In the next step, a 16-bit digital signal processor (DSP) manages temperature compensation. Finally, the signal is converted back into an analog output. Delivering an analog output allows direct-replacement compatibility with standard existing sensors while providing the advantages of a new MEMS device.
The MLX90830 features configurable diagnostics for tailored monitoring and troubleshooting, and the IC boasts ± 0.5% full-scale lifetime accuracy and fast response times of just 0.4 ms. In addition, the Melexis MLX90830 meets AEC-Q100 and AEC-Q103-002 certifications and is ASIL compliant. Developed as an ASIL A SEooC (ISO 26262) device, it ensures a high level of safety and reliability in automotive applications.
To learn more about the Melexis MLX90830 Triphibian MEMS pressure sensor IC, visit https://www.mouser.com/new/melexis/melexis-mlx90830-sensors/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
2026 - Melexis - Combining a passion for technology with truly inspired engineering, Melexis designs, develops and delivers innovative micro-electronic solutions that enable designers to turn ideas into applications that support the best imaginable future. The company’s advanced mixed-signal semiconductor sensor and actuator components address the challenges of integrating sensing, driving and communication into next-generation products and systems that improve safety, raise efficiency, support sustainability and enhance comfort.
Melexis is headquartered in Belgium and employs over 1,500 people in 19 locations worldwide.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.