Mouser Signs Global Distribution Agreement with Macronix to Stock Wide Range of High-Performance Memory Products

För omedelbar lansering

Anslut till oss


April 1, 2023Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, today announced it has entered into a distribution agreement with Macronix International Co., Ltd., a leading provider of non-volatile memory solutions. Macronix designs and manufactures an expansive range of NOR Flash and NAND Flash products for diverse applications from computing, consumer, networking, and industrial to mobile, embedded, automotive, medical devices and Internet of Things (IoT).

"Macronix's world-class portfolio of unique, high-performance products aligns well with our line card and customer base," said Kristin Schuetter, Vice President of Supplier Management at Mouser Electronics. "We look forward to providing engineers and buyers worldwide with their innovative embedded memory solutions, backed by Mouser's best-in-class logistics and unsurpassed customer service."

"Macronix is a leader in non-volatile memories, and we are excited to partner with Mouser to expand our presence in the market," said J.T. Chung, Vice President of Worldwide Sales at Macronix. "With Mouser's world-class distribution channel and support, we are confident we will be able to enhance our customer base as well as expand our reach globally. We look forward to a long and successful partnership with Mouser."

Mouser is stocking a wide range of Macronix memory solutions. The MX25S 1.2V serial NOR flash offers ultra-low power consumption, effectively extending battery life. MX25S components are provided in densities from 4Mb to 128Mb and offered in compact packages, such as USON, WLCSP or Known Good Die (KGD), that can be used with system-in-package (SiP) solutions. These devices are ideal for health monitoring applications, wireless devices, IoT, wearables and more.

Macronix MX25R ultra-low power serial NOR flash is a family of memory products with a wide range voltage input range (1.65V to 3.6V), suitable for use in a wide variety of IoT and other energy-conscious applications, such as wearable and mobile devices.

The MX25Ux/MX66Ux 1.8V and MX25Lx/MX66LM 3V OctaFlash™ NOR flash, also available from Mouser, are extreme speed memory products built on a serial peripheral interface (SPI) and command protocol, providing extendable I/O capability. Macronix OctaFlash, built on OctaBus™ technology, is ideal for bus sharing, which enables simplicity in system design while optimizing PCB space, resulting in significant cost savings. These NOR flash devices are an ideal solution for over-the-air (OTA) update applications, which are becoming more prevalent within automotive and IoT solutions.

To learn more about Macronix memory solutions available from Mouser, visit https://www.mouser.com/manufacturer/macronix/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Macronix

2026 - ​​​​​​​​​​​​Macronix is a leading integrated device manufacturer in the Non-Volatile Memory (NVM) market. The company provides a full range of NOR Flash, NAND Flash, and ROM products. With its world-class R&D and manufacturing capability, Macronix continues to deliver high-quality, innovative, and performance-driven products to its customers in the consumer, communication, computing, industrial, automotive, networking, and other segment markets.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764