Mouser Electronics Teams Up with MacroFab to Sponsor the Food Device Design Derby Challenge
February 21, 2024 – Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, today announces that it is sponsoring a new electronics design competition presented by MacroFab, an operator of one of North America's largest technology platforms for electronics manufacturing. To speed time to market for its customers, MacroFab provides a software-driven approach to custom PCB design, prototyping and manufacturing.
In MacroFab's Food Device Design Derby Challenge, entrants will be tasked to create something that combines electronics with food, whether it's a gadget to enhance cooking skills, an automated herb garden, or sensors that let the user know when cooking is completed. Entrants are required to document their creation, including inspiration, design process, power requirements, and any source code and schematics. Entrants need to post their project on MacroFab's Circuit Break Discussion community site under the Contest Category. Then, upload it to MacroFab's platform and complete the Bill of Materials and specifications. Also, entrants should post in the Circuit Break discussion thread or on a public repository, such as GitHub, with all documentation so that the project is replicable.
The contest runs now until 8 AM CST, March 31, 2024. The first-place prize is $2,000; second-place winner receives $1,000; and third-place is $500. A special $2,000 prize will be awarded to the favorite entry of the Circuit Break Podcast. In addition, MacroFab will be giving away themed trophies and free prototyping worth up to $1,200. The contest has no age limit; however, anyone affiliated with MacroFab, Mouser Electronics, or the judges (or those related to them) is ineligible to participate.
Previous MacroFab design competitions sponsored by Mouser include the Useless Machine Challenge and the Blink an LED Contest.
To learn more about the Food Device Design Derby Challenge, visit https://www.macrofab.com/events/macrofab-food-device-design-derby-challenge/.
About MacroFab
2024 - MacroFab operates the largest technology platform for electronics manufacturing from prototype to high-scale production, with a network of 100+ factories across North America. The company's technology-enabled manufacturing platform and marketplace enable faster, more efficient electronics production, closer to end-users while leveraging AI-enabled sourcing opportunities, expert internal teams, and an easy-to-use platform. The company is headquartered in Houston, TX. For more details, visit https://www.macrofab.com/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.