Mouser and Molex Sponsor IndyCar Team Running in Indy 500

The Greatest Spectacle in Motorsports Returns with Fans
För omedelbar lansering

Anslut till oss


Mouser and Molex Sponsor IndyCar Team Running in Indy 500

May 25, 2021 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader empowering innovation, together with valued supplier Molex, is gearing up for this year's Indianapolis 500 at the legendary Indianapolis Motor Speedway. The team competed at the historic track in last weekend's GMR Grand Prix, where the "Mouser Machine" made its 2021 debut for the Dale Coyne Racing with Vasser Sullivan team, sporting a Mouser Blue livery. They made it to Round 2 of qualifying and ultimately came home with a Top 15 finish.

Ed Jones, the driver of the No. 18 car, and the entire racing team now turn their attention to the 105th running of the Indianapolis 500 which will take place on May 30. The full spectacle is almost two weeks long, with multiple practices and qualifying sessions ultimately leading up to the big day.

"We are excited to see Ed Jones behind the wheel at this year's Indy 500 for the Vasser Sullivan team," said Todd McAtee, Mouser Electronics' Vice President, Americas Business Development. "It would be so thrilling to have another Indy 500 victory like we did in 2013. The collaboration between the team, Mouser and Molex is a testament to our combined mission for excellence."

Mouser Electronics, an industry's leading distributor with the widest selection of semiconductors and electronic components, is proud to again team up with valued supplier Molex to sponsor Jones and the Dale Coyne Racing with Vasser Sullivan team for the entire 2021 NTT IndyCar Series.

Mouser first sponsored IndyCar racing in 2011 as an inventive way to communicate its performance-driven business model and promote the newest technologies. The Mouser- and Molex-sponsored car won the Indianapolis 500 in 2013, as well as the 2017 and 2018 series-opening races at St. Petersburg, Florida.

The Indy 500 will be televised on NBC in the U.S., Sunday, May 30. After the Indianapolis 500, the IndyCar series travels to Detroit for the second doubleheader of the season on June 12 and 13. The series then closes out the season with eight more races, ending with the season finale in Long Beach, California, on September 26.

For more information, visit https://www.mouser.com/indy-racing/.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764