Mouser Electronics Continues to Expand its Industrial Automation Line Card and Product Lineup

För omedelbar lansering

Anslut till oss


December 17, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components, continues to expand its line card of industrial automation products from world-class manufacturers and solution delivery partners, helping to pave the way for Industry 5.0

The transition to Industry 5.0 marks a significant evolution in the manufacturing sector, heralding a new era that goes beyond the automation and digitalization of Industry 4.0 by integrating human creativity with technological advancements.

The PE2100U from ASUS IoT is an intelligent edge computer featuring rich I/O capabilities, various connectivity options and a fanless thermal design suitable for diverse industrial control applications. Based on Intel® 13th Gen. Core™-I processors, these rugged embedded computers include up to 4 COM ports, provide triple independent video outputs (2x HDMI 2.0 / 1x DP 1.2), and offer plentiful expansion capacity. The PE2100U industrial PCs support Wi-Fi®, Bluetooth®, and multiple wired connectivity options.

The LOGO! 8.4 logic modules from Siemens are cloud-enabled, space-saving interfaces for connecting expansion modules in industrial automation, predictive maintenance, and agricultural applications. The Siemens LOGO! Soft Comfort engineering software wizard facilitates both single and network cloud connections with familiar and easy operation, featuring automatic communication configuration for up to three programs at once, with drag-and-drop transfer signals from one program to another.

The K50Z multipoint sensor from Banner Engineering uses 3D time-of-flight (ToF) technology and a wide beam angle to detect objects up to 2 meters away across an 8 x 8-pixel array. It can also be configured to measure two separate areas, effectively doing the work of two sensors in one convenient device. The K50Z sensor is completely self-contained, and no external lighting, controller, or PC is required. The K50Z sensor has a compact IP67 housing designed for industrial environments and is ideal for fill applications or area detection.

The SLC Safety Light Curtain series by TE Connectivity is designed to provide operator safety while allowing quick and safe access for various operations such as loading, unloading, and maintenance. These curtains offer resolutions ranging from 14 to 90 millimeters, making them suitable for detecting fingers, hands, or the entire body. They also come with 2 to 4-beam options for effective access control. These curtains offer resolutions ranging from 14 to 90 millimeters, making them suitable for detecting fingers, hands, or the entire body.

To provide expert insights into Industry 4.0 and Industry 5.0, Mouser has curated a library of educational resources for engineers, buyers and systems integrators through its comprehensive industrial automation resource hub, featuring a diverse array of educational materials, including articles, blogs, product profiles, and more. In collaboration with leading industry experts, Mouser has also developed informative eBooks that explore key topics such as IIoT, advancements in digital factories, and future industry trends. These manufacturer eBooks are meticulously designed to equip engineers and designers with the latest knowledge and applications, ensuring they remain at the forefront of technological innovation.

To learn more about Mouser's industrial automation portfolio, visit https://www.mouser.com/solutions/industrial-automation/.

 

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764