Mouser-Sponsored Vasser Sullivan Lexus Racing Team Tackles Mobil 1 Twelve Hours of Sebring IMSA Race

För omedelbar lansering

Anslut till oss


March 6, 2025 - Mouser Electronics, Inc.,  the New Product Introduction (NPI) leader™ empowering innovation, is excited to cheer on the Vasser Sullivan Lexus Racing team at the Mobil 1 Twelve Hours of Sebring Endurance Race on March 15 in Sebring, Florida.

The Mobil 1 Twelve Hours of Sebring offers a long weekend of racing action, with two days of practice and qualifying sessions leading up to the 12-hour race on Saturday. Sebring International Raceway will play host to the festivities, which is a 3.74-mile-long track boasting 17 corners. It is one of the oldest continuously operating racetracks in North America and was originally built as part of Hendricks Army Airfield, a WWII training base for B-17 pilots. The track's most defining feature is its famous, high-speed "Turn 17," a long, fast right-hander that can make or break a car's speed down the front straight. The corner, which can fit up to three cars wide, is also known as "Sunset Bend" because as night falls on the 12-hour race, drivers are looking right into the setting sun heading into the turn. The track also features a "safety pin" turn and the "Gendebien Bend," which is designed to slow the cars' entry to the Ullman straightaway. The track surface has 3.04 miles of asphalt and 0.7 miles of concrete and is notoriously bumpy due to its airfield origins.

The No. 14 Lexus RC F GT3 will be piloted by drivers Ben Barnicoat, Aaron Telitz, and Kyle Kirkwood, while Jack Hawksworth, Parker Thompson, and Frankie Montecalvo will be co-driving the No. 12 Lexus entry in the GTD class.

Mouser and valued manufacturer partner Molex co-sponsor the Vasser Sullivan Lexus Racing team, seeing the opportunity as an inventive way to communicate its performance-driven business model and promote the newest technologies.

Visit https://www.mouser.com/imsa-racing/ for more information on Mouser's sponsorship of the Vasser Sullivan Lexus Racing team and to see the schedule for the 2024 season.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764