Mouser-Sponsored Vasser Sullivan Lexus Racing Team Nears IMSA Season-End at the Racing Capital of The World

För omedelbar lansering

Anslut till oss


September 13, 2023Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is ready to cheer on the Vasser Sullivan Lexus Racing team as they head to the Racing Capital of The World, Indianapolis Motor Speedway (IMS), in Indianapolis, IN, for the Battle on the Bricks on September 17.

The Vasser Sullivan Lexus Racing team is hoping for a strong finish in the season's penultimate race. The full-time driver lineups for Vasser Sullivan Racing include Jack Hawksworth and Ben Barnicoat in the No. 14 Lexus RC F GT3 in the GTD PRO class, with Aaron Telitz and Frankie Montecalvo co-driving the No. 12 Lexus entry in the GTD class.

The Vasser Sullivan Lexus Racing team is currently in first place in the GTD PRO class standings with 3,165 points and third place in the GTD class standings with 2,553 points.

The Indianapolis Motor Speedway course is 2.439 miles long and has 14 turns. This will be the first time IMSA is racing at IMS since the 2014 season (the first ever IMSA race held there was in 2012). Indianapolis Motor Speedway is steeped in history, built initially using hand-laid bricks in 1909, leading to its nickname, "The Brickyard." The Indianapolis Motor Speedway is the world's third oldest permanent automobile racetrack and was designated a National Historic Landmark in 1987, the only such site affiliated with automotive racing history.

Mouser and valued manufacturer partner Molex co-sponsor the Vasser Sullivan Lexus Racing team, seeing the opportunity as an inventive way to communicate its performance-driven business model and promote the newest technologies.

After the Battle on the Bricks, the season finale race will be the Motul Petit Le Mans at Road Atlanta on October 14 in Braselton, Georgia.

For more information on Mouser's sponsorship of the Vasser Sullivan Lexus Racing team and to see the schedule for the 2023 season, visit https://www.mouser.com/imsa-racing/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764