Mouser-Sponsored Vasser Sullivan Lexus Racing Team Wins IMSA 2023 GTD PRO Title

För omedelbar lansering

Anslut till oss


October 26, 2023Mouser Electronics, Inc., congratulates the Vasser Sullivan Lexus Racing team for winning the 2023 IMSA WeatherTech SportsCar Championship GTD PRO Manufacturers Championship at the Petit Le Mans at Michelin Raceway Road Atlanta on October 14, with 3760 total points. Drivers Ben Barnicoat and Jack Hawksworth also won the GTD PRO Drivers title and the GTD PRO Team championship.

"Congratulations to the entire Vasser Sullivan Lexus Racing team on an outstanding season. Our compliments to drivers Jack and Ben for their GTD PRO title wins and to Aaron and Frankie for taking third place in the championship for GTD class," said Todd McAtee, Senior Vice President, Business Development for Mouser Electronics. "What a thrilling year. We are so proud to support this talented group."

The GTD PRO team scored two victories throughout the season, with an additional seven podiums to sweep the driver, team and manufacturer championships. Hawksworth also led the GTD PRO class with four pole positions this year. This marks the first full-season IMSA GT titles for Lexus and Vasser Sullivan, as well as for Hawksworth and Barnicoat. Endurance racers Kyle Kirkwood and Mike Conway also contributed to the manufacturer’s title with endurance race starts in the Lexus RC F GT3 this season.

Additionally, drivers Aaron Telitz and Frankie Montecalvo finished the 2023 season in third place in the IMSA GTD championship, with 2927 points. They were joined by endurance racer Parker Thompson during the four endurance events this year. The highlight of the season for the GTD drivers came at Watkins Glen International in June when the trio dominated and won the six-hour endurance event, giving the Vasser Sullivan Lexus Racing team the first double victory in program history.

The 2023 IMSA season marked the fifth year Lexus and Vasser Sullivan have partnered together. During that time, the Vasser Sullivan Lexus RC F GT3s have earned an impressive 13 wins, 39 podiums and 18 pole positions. Mouser and valued manufacturer partner Molex co-sponsor the Vasser Sullivan Lexus Racing team, seeing the opportunity as an inventive way to communicate its performance-driven business model and promote the newest technologies.

The 2024 IMSA WeatherTech SportsCar Championship season will kick off on January 27 and 28, with the Rolex 24 at the Daytona International Speedway, in Daytona, Florida.

To learn more about the Vasser Sullivan Lexus Racing team, and to preview the 2024 schedule, visit https://www.mouser.com/imsa-racing/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764