Mouser-Sponsored DS PENSKE Formula E Racing Team Readies for Inaugural Shanghai E-Prix in China

För omedelbar lansering

Anslut till oss


Learn more about the DS PENSKE Formula E racing team
Photo: DPPI

May 21, 2024 - Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is excited to cheer on the DS PENSKE Formula E racing team for the first time in Shanghai, China, for rounds 11 and 12 of the Season 10 ABB FIA Formula E World Championship. The weekend gets started on May 25 for round 11 and continues on May 26 for round 12.

The DS PENSKE team is coming off another doubleheader weekend in Berlin, Germany, where Jean-Éric Vergne claimed another podium finish in round 9. The Shanghai races will take place at the Shanghai International Circuit, which opened in 2004. The track layout was inspired by Chinese culture, with the designers claiming to have drawn inspiration from the Chinese “shang” symbol for the overall configuration. The track is comprised of 12 turns and is 3.051 km in length. With a right-left-right chicane section, hairpin turns, and an open straightaway, the circuit is sure to provide some excitement for the inaugural Shanghai E-Prix. The DS PENSKE team is currently in 4th place for the 2024 season championship with 127 points. Team drivers for this season are Season 8 Champion Stoffel Vandoorne and two-time Formula E Champion Jean-Éric Vergne.

Mouser is supporting the DS PENSKE team for the globe-trekking 2024 season in collaboration with TTI, Inc. and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.

Formula E is an international, fully electric street racing series. Using the very latest technology, the DS Performance Team has stretched the boundaries of efficiency and performance with the DS E-TENSE-FE23 powertrain and software. Racing is all about speed and endurance, and racing sponsorships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

To learn more about the Mouser-backed DS PENSKE Formula E team and view the 2024 Formula E schedule, visit https://www.mouser.com/formula-e/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764