Mouser-Sponsored Formula E Racing Team Heads for Portland Doubleheader in the USA

För omedelbar lansering

Anslut till oss


June 25, 2024 - Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is excited to support the DS PENSKE Formula E racing team in Portland, Oregon, USA, for rounds 13 and 14 of the Season 10 ABB FIA Formula E world Championship. The doubleheader weekend starts on June 29 for round 13 and continues on June 30 for round 14.

The DS PENSKE team is hoping to carry some momentum from the Shanghai E-Prix, where two-time Formula E Champion Jean-Éric Vergne captured pole position for round 11 and 2022 World Champion Stoffel Vandoorne finished in sixth position for round 12. The races in Portland, Oregon, will serve as the home races for the team this year, as this is the only stop of the season in the USA. The Portland International Raceway will play host to the weekend-long festivities. The permanent circuit is 3.190 km in length and has 12 turns. PIR is a familiar stop for American motorsports such as IndyCar, and the layout tends to lead to a lot of excitement. The Formula E series debuted here last season and had a record number of overtakes. Portland International Raceway sits on roughly 268 acres of land, 83 of which are part of an environmental protection zone.

Mouser is supporting the DS PENSKE team for the globe-trekking 2024 season in collaboration with TTI, Inc. and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.

Formula E is an international, fully electric street racing series. Using the very latest technology, the DS Performance Team has stretched the boundaries of efficiency and performance with the DS E-TENSE-FE23 powertrain and software. Racing is all about speed and endurance, and racing sponsorships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

To learn more about the Mouser-backed DS PENSKE Formula E team and view the 2024 Formula E schedule, visit https://www.mouser.com/formula-e/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764