Mouser-Backed DS PENSKE Formula E Racing Team Returns to Miami for Round 5 of the ABB FIA Formula E World Championship

För omedelbar lansering

Anslut till oss


April 9, 2025 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is ready to support the DS PENSKE Formula E team as they come to the United States for round 5 of Season 11 of the ABB FIA Formula E World Championship. This is the only US stop for Season 11, and it will take place in Miami, Florida, at Homestead-Miami Speedway on April 12.

The 2025 Miami E-Prix at Homestead-Miami Speedway will be the first return to Miami since it hosted the first Formula E race on US soil in the inaugural 2015 season. Opening in 1995, the track has played host to every major North American race series, from NASCAR to IMSA and IndyCar, and once again, Formula E. As the track echoes the Art Deco glitz of nearby Miami Beach, splashes of turquoise, purple, and silver will make an excellent backdrop to what is sure to be an exciting race weekend.

The DS PENSKE Formula E team is led by two-time Formula E Champion Jean-Éric Vergne and Maximilian Günther as they pilot the new GEN3 Evo car. The GEN3 Evo is faster, stronger, and more agile than its predecessors and features an aggressive new body kit designed to be stronger, more robust and more aerodynamic. The new GEN3 Evo cars can go from 0-60 mph in 1.82 seconds, 30% faster than an F1 car. It also allows for all-wheel drive, a first for a Formula E car.

Mouser is supporting the DS PENSKE team for the globe-trekking 2024/2025 season in collaboration with TTI, Inc., and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.

Formula E cars are powered solely by electricity and represent a vision for the future of the motorsports industry, serving as a framework for research and development around zero-emission motoring. Racing is all about speed and endurance, and racing partnerships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

To learn more about the Mouser-backed DS PENSKE Formula E team and view the ABB FIA Formula E World Championship Racing Season 11 schedule, visit https://www.mouser.com/formula-e/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764