Mouser-Backed DS PENSKE Formula E Racing Team Readies for Mexico City E-Prix
January 7, 2025 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is ready to cheer on the DS PENSKE Formula E racing team as they head to Mexico City, Mexico, for round 2 of the 2024/2025 ABB FIA Formula E World Championship racing season. The Hankook Mexico City E-Prix will take place on January 11, 2025.
The DS PENSKE Formula E racing team is led by two-time Formula E Champion Jean-Éric Vergne and Maximilian Günther as they pilot the new GEN3 Evo car. The GEN3 Evo is faster, stronger, and more agile than its predecessors and features an aggressive new body kit designed to be stronger, more robust and more aerodynamic. It also allows for all-wheel drive, a first for a Formula E car.
The Mexico City course is one of the fastest tracks on the calendar. As a fan favorite, the track always makes use of the legendary Autodromo Hermanos Rodriguez circuit. Starting on the traditional start/finish straight, the Formula E grid will shoot down into turn one. After a long and fast Turn 2, the pack will make their way around Turn 3, which breaks off left into a four-turn sequence. Looping back around a hairpin, Turns 6 and 7 get technical, with a straight and sharp right-hand bend leading into a chicane complex for a quick blast into the legendary Foro Sol stadium section. Leaving the stadium, the drivers will then jostle for position out of the iconic Peraltada curve in the run to the finish line.
Mouser is supporting the DS PENSKE team for the globe-trekking 2024/2025 season in collaboration with TTI, Inc. and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.
Formula E cars are powered solely by electricity and represent a vision for the future of the motorsports industry, serving as a framework for research and development around zero-emission motoring. Racing is all about speed and endurance, and racing partnerships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.
To learn more about the Mouser-backed DS PENSKE Formula E racing team and view the ABB FIA Formula E World Championship Racing Season 11 schedule, visit https://www.mouser.com/formula-e/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.