Mouser-Backed DS PENSKE Formula E Racing Team Readies for Doubleheader in London
July 26, 2023 – Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is excited to watch the DS PENSKE Formula E Racing Team as they look to end the season on a high note for the final races of the season at the London E-Prix doubleheader, on July 29th and 30th.
The London races feature a unique track that weaves its way inside and outside the exhibition center and around the historical heartland of the Royal Docklands. The ExCel Circuit is motorsport’s only indoor and outdoor race circuit, made possible by the emissions-free nature of the cars. The track features 20 turns with a total length of 2.09 KM. Drivers and teams will have to deal with two different surface types: the smooth indoor surface with more grip and the abrasive asphalt on the outdoor portion, plus elevation and lighting changes, presenting unique challenges.
Team drivers for the race are two-time Formula E Champion Jean-Éric Vergne and Season 8 Champion Stoffel Vandoorne. The DS PENSKE Formula E Racing Team is currently fifth in the ABB FIA Formula E World Championship, with 153 points.
Mouser is supporting the DS PENSKE team for the globe-trekking 2022–23 season, in collaboration with TTI, Inc. and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.
Earlier this year, Formula E was independently ranked and recognized as the most sustainable sport in the world by the Global Sustainability Benchmark in Sports (GSBS), in addition to maintaining the International Standard for Sustainable Events (ISO 20121) and the FIA Three-Star level for Environmental Accreditation.
Using the very latest technology, the DS Performance Team has stretched the boundaries of efficiency and performance with the DS E-TENSE powertrain and software. Racing is all about speed and endurance, and racing sponsorships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.
To learn more about the Mouser-backed DS PENSKE Formula E team, visit https://www.mouser.com/formula-e/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.