Mouser-Backed DS PENSKE Formula E Racing Team Prep for Doubleheader in Jeddah, Saudi Arabia
February 11, 2025 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is excited to cheer on the DS PENSKE Formula E racing team as it competes in rounds 3 and 4 of Season 11 of the ABB FIA Formula E World Championship at the Jeddah Corniche Circuit in Jeddah in Saudi Arabia on February 14 and 15, 2025. This will be the first time that Formula E has raced at Jeddah, and with its breathtaking Red Sea backdrop, the E-Prix promises to be an unforgettable experience for fans and competitors alike.
The Jeddah Corniche Circuit is the same venue used by the Saudi Arabian Grand Prix in Formula One but will be modified to a 3.001 km (1.865 mi), 19-turn format to accommodate Formula E. To add to the excitement, the two races will be run at night with the illumination of LEDs lining the track and on the cars.
The Jeddah race is also going to include the introduction of PIT BOOST to Formula E. PIT BOOST is an innovative mid-race feature that provides a 10% energy increase (3.85kWh) to race cars through a 34-second, 600kW rapid recharge in the pit lane. Each driver must choose the optimal moment to use PIT BOOST, adding an extra layer of drama to every race. Designed to enhance strategy, unpredictability and fan engagement, PIT BOOST will showcase cutting-edge EV ultra-fast recharging technology while adding a thrilling new dimension to Formula E races.
The DS PENSKE Formula E racing team is led by two-time Formula E Champion Jean-Éric Vergne and Maximilian Günther as they pilot the new GEN3 Evo car. The GEN3 Evo is faster, stronger, and more agile than its predecessors and features an aggressive new body kit designed to be stronger, more robust and more aerodynamic. It also allows for all-wheel drive, a first for a Formula E car.
Mouser is supporting the DS PENSKE team for the globe-trekking 2024/2025 season in collaboration with TTI, Inc. and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.
Formula E cars are powered solely by electricity and represent a vision for the future of the motorsports industry, serving as a framework for research and development around zero-emission motoring. Racing is all about speed and endurance, and racing partnerships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.
To learn more about the Mouser-backed DS PENSKE Formula E racing team and view the ABB FIA Formula E World Championship Racing Season 11 schedule, visit https://www.mouser.com/formula-e/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.