Mouser-Backed DS PENSKE Formula E Racing Team Looks to Keep the Momentum Going for Jakarta E-Prix

För omedelbar lansering

Anslut till oss


June 18, 2025 — Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is proud to support the DS PENSKE Formula E team as they head to the Indonesian capital of Jakarta for round 12 of the Season 11 ABB FIA Formula E World Championship on June 21. Team drivers for the Jakarta race are Maximilian Günther and two-time Formula E Champion Jean-Éric Vergne, fresh off a spectacular 1st and 2nd Place Double Podium in Shanghai.

The 2.37 km Jakarta E-Prix track was largely purpose-built for the Formula E race, debuting in 2022. The circuit includes 18 turns and features a horse-like design inspired by the traditional Javanese Kuda Lumping dance, which portrays troops riding horses. The turn 13 hairpin is the most demanding braking zone on the track, sure to test every aspect of car and driver performance.

The DS PENSKE team will be driving the new GEN3 Evo car, which is faster and more agile than its predecessors and features an aggressive new body kit designed to be stronger, more robust and more aerodynamic. The new GEN3 Evo cars can go from 0-60 mph in 1.82 seconds, 30% faster than an F1 car. It also allows for all-wheel drive, a first for a Formula E car.

Mouser is supporting the DS PENSKE team for the globe-trekking 2024/2025 season in collaboration with TTI, Inc., and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.

Formula E cars are powered solely by electricity and represent a vision for the future of the motorsports industry, serving as a framework for research and development around zero-emission motoring. Racing is all about speed and endurance, and racing partnerships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

To learn more about the Mouser-backed DS PENSKE Formula E team and view the ABB FIA Formula E World Championship Racing Season 11 schedule, visit https://www.mouser.com/formula-e/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764