Mouser-Backed Formula E Team Carries Top-10 Momentum into Germany for Series Finale

Molex, TTI, and AVX Join Mouser to Support All-Electric Racing
För omedelbar lansering

Anslut till oss


August 11, 2021 – Fresh from a dual top-10 finish at the London E-Prix, the Mouser Electronics-supported Formula E racing team will close out the 2020–21 championship season at the Berlin E-Prix, August 14 and 15. Mouser will be cheering on the DRAGON / PENSKE AUTOSPORT team and drivers Joel Eriksson and Sérgio Sette Câmara as they race along the giant apron section of Berlin’s historic Tempelhof Airport.

Mouser has partnered with the team throughout the 2020–21 ABB FIA Formula E Championship racing season, in collaboration with TTI, Inc. and valued manufacturers Molex and AVX. This is the seventh-straight year that Mouser and Molex have sponsored Formula E racing.

Eriksson and Sette Câmara, both of whom finished in the top 10 in the second London E-Prix race, will tackle the high-grip surface of the Tempelhof street circuit while the team nimbly adjusts race strategies to maintain energy and speed.

The Formula E series features cars that are powered solely by electricity and represent a vision for the future of the motor sports industry, serving as a framework for research and development around zero-emission motoring. The Gen2 cars offer a huge step forward in electric vehicle racing technology, with maximum power of 250 kW and speeds up to 280 km/h. Racing is all about speed and endurance, and racing sponsorships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

Fans can cast a vote for Eriksson and Sette Câmara in FANBOOST, which allows fans to play an active role in influencing the outcome of the race. FANBOOST gives fans the opportunity to vote for their favorite driver and award them an extra boost of power during the race. The five drivers with the most FANBOOST votes are awarded a significant burst of power, which they can deploy in a 5-second window during the second half of the race. FANBOOST voting for the Berlin E-Prix opened August 11 and is available up to 15 minutes into the race.

For more information about Formula E and to register and vote in FANBOOST, visit https://www.mouser.com/formula-e.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764