Mouser-Backed DS PENSKE Formula E Racing Team Returns to Historic Tempelhof Airport in Berlin for Doubleheader
July 9, 2025 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is ready to cheer on the DS PENSKE Formula E racing team in Berlin, Germany, for rounds 13 and 14 of the Season 11 ABB FIA Formula E World Championship. The race weekend will kick off on July 12.
The Berlin races will again occur at the historic Tempelhof Airport, known for its abrasive track surface. The repeating concrete slabs that make up much of the track require drivers to adjust their strategies to deal with energy management and tire wear. The track was largely reconfigured in 2024 to better suit the speed and characteristics of the Gen3 cars. Spanning 2.343km, the amended Tempelhof circuit introduced five new turns, including a tight hairpin at the center of the circuit.
The DS PENSKE Formula E team is led by Maximilian Günther and two-time Formula E Champion Jean-Éric Vergne as they pilot the new GEN3 Evo car. The GEN3 Evo is faster, stronger, and more agile than its predecessors and features an aggressive new body kit designed to be stronger, more robust and more aerodynamic. The new GEN3 Evo cars can go from 0-60 mph in 1.82 seconds, 30% faster than an F1 car. It also allows for all-wheel drive, a first for a Formula E car.
Saturday's race will include PIT BOOST, an innovative mid-race feature that provides a 10% energy increase (3.85 kWh) to race cars through a 34-second, 600 kW rapid recharge in the pit lane. Each driver must choose the optimal moment to use PIT BOOST, adding an extra layer of drama to every race. Designed to enhance strategy, unpredictability and fan engagement, PIT BOOST showcases cutting-edge EV ultra-fast recharging technology while adding a thrilling new dimension to Formula E races.
The Berlin Formula E weekend will also feature a Rookie Test race, with Nikita Bedrin driving for DS PENSKE. Bedrin has previously raced in karting and single-seaters and recently captured his first FIA Formula 3 Sprint Race victory in 2024. Bedrin’s first on-track experience with DS PENSKE, on July 14, will give him a unique opportunity to familiarize himself with the demands of all-electric racing.
Mouser supports the DS PENSKE team for the globe-trekking 2024/2025 season in collaboration with TTI, Inc., and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.
Formula E cars are powered solely by electricity and represent a vision for the future of the motorsports industry, serving as a framework for research and development around zero-emission motoring. Racing is all about speed and endurance, and racing partnerships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.
To learn more about the Mouser-backed DS PENSKE Formula E team and view the ABB FIA Formula E World Championship Racing Season 11 schedule, visit https://www.mouser.com/formula-e/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.