Now at Mouser: Espressif Systems ESP32-S3-BOX-3 Next-Generation Open-Source AIoT Kit

Nya produktlanseringar

Anslut till oss


June 24, 2024—Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is stocking ESP32-S3-BOX-3 next-generation open-source AIoT kit from Espressif Systems. This AI development kit is ideal for developers looking to prototype and transform existing factory operating systems into Edge, AI and HMI applications or other complex IoT systems.

The Espressif Systems ESP32-S3-BOX-3 open-source AIoT kit, available from Mouser, is a feature-rich development tool based on the ESP32-S3 Wi-Fi® + Bluetooth® 5 Low Energy system-on-chip (SoC) featuring AI acceleration capabilities. The SoC also features 512KB SRAM, supported by 16MB of quad flash and 16MB of octal PSRAM. The kit also contains a 2.4-inch (320 x 240) SPI touchscreen, two digital microphones, a speaker, a USB Type-C™ port, and a high-density PCIe connector for hardware expansion. The ESP32-S3-BOX-3 delivers a speech-recognition framework that provides users with an offline AI voice assistant with far-field voice interaction, continuous recognition, wake-up interruption, and the ability to recognize over 200 customizable command words.

The ESP32-S3-BOX-3 is a versatile device that supports the Matter protocol, enabling users to utilize it as a Matter-over-Wi-Fi/Thread end-device, a Thread border router, or a Matter gateway. Additionally, the ESP32-S3-BOX-3 supports working with the open-source, home-automation platform and home assistant, thus providing users with a powerful, local home controller that rivals Amazon Echo and Google Home. The outstanding AI capabilities and low power consumption of the ESP32-S3-BOX-3 make it the ideal choice for smart home automation, delivering seamless connectivity and effortless control over a wide range of devices.

Espressif’s AIoT Cloud platform, ESP RainMaker®, can be used with ESP32-S3-BOX-3 to configure GPIOs and offline voice commands while also offering remote control via phone apps or third-party voice assistants. Espressif’s ESP Insights software provides a remote diagnostics solution to monitor the functioning of the ESP32-S3-BOX-3 in the field, thus ensuring optimal performance at all times.

To learn more, visit https://www.mouser.com/new/espressif/espressif-esp32-s3-box-3-kit/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About Espressif Systems

2026 - Espressif Systems is an advanced and professional IC design company that provides low-power Wi-Fi and Bluetooth SoCs and wireless solutions for Internet of Things (IoT) applications. The company has a team of innovators from around the world, working in the areas of chip design, algorithm research, software development, open source development, product development, and customer services.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764