New at Mouser: Espressif Systems ESP32-C61 Wi-Fi 6 + Bluetooth 5 (LE) SoC for IoT, Industrial, Robotics, and Smart Applications
February 9, 2026 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new ESP32-C61 Wi-Fi® 6 + Bluetooth® 5 (LE) System-on-Chip (SoC) from Espressif Systems. The ESP32-C61 SoC is designed for IoT, smart home, industrial, robotics, sensor, and medical device applications.
The Espressif Systems ESP32-C61 SoC, available from Mouser, features optimized peripherals and improved connectivity, powered by a 32-bit RISC-V processor running at up to 160 MHz, including external PSRAM support. This enables developers to build feature-rich applications, allowing for larger data buffers, additional functionality, and future upgrades with less time spent on memory optimization. The ESP32-C61 supports a 20MHz bandwidth for 802.11ax mode and a 20MHz/40MHz bandwidth for 802.11b/g/n mode, featuring characteristics, such as OFDMA and MU-MIMO for reliable and low-latency connections, as well asl target wake time (TWT) for ultra-low power applications. Additionally, the ESP32-C61 chip incorporates a robust set of peripherals, including SPI, I2C, UART, I2S, ADC, GDMA, ETM, and an analog comparator. The Bluetooth 5 (LE) radio enables long-range operation via advertisement extension and a coded PHY, while supporting a high-throughput PHY of 2 Mbps. The ESP32-C61 also supports the BLE Mesh 1.1 protocol, ESP-IDF, and the ESP-Matter SDK, or can operate as a wireless co-processor through ESP-AT or ESP-Hosted, facilitating seamless integration into various system architectures.
The ESP32-C61 features secure boot, flash, and PSRAM encryption with cryptographic accelerators and has an ECDSA-based digital signature peripheral (DSP) in hardware, thus safeguarding private keys from software access. The addition of a trusted execution environment (TEE), utilizing access permission management (APM), a hardware block, and physical memory protection (PMP), provides mechanisms for software isolation.
To learn more, visit https://www.mouser.com/new/espressif/espressif-esp32-c61-socs/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
2026 - Espressif Systems is an advanced and professional IC design company that provides low-power Wi-Fi and Bluetooth SoCs and wireless solutions for Internet of Things (IoT) applications. The company has a team of innovators from around the world, working in the areas of chip design, algorithm research, software development, open source development, product development, and customer services.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.