Mouser Electronics and Samtec Present Webinar on Signal Integrity in Embedded Applications
04 October 2023 – Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, has teamed up with Samtec to offer the engineering community a free webinar titled “An Introduction to Signal Integrity in Embedded Computing Applications”. The webinar will be streamed live on Tuesday, 24 October at 17:00 CEST.
For embedded developers, challenges related to interference on the board are becoming more common. Embedded technologies are now increasingly using high-speed communication protocols such as PCI Express®, Ethernet and USB. It is therefore important for designers to understand fundamental signal integrity (SI) principles. Attendees will learn how to optimise SI in embedded applications and work through practical examples in real-world case studies.
Participants attending the webinar will learn how to:
- Develop a fundamental understanding of key SI parameters
- Explore SI principles for common embedded computing protocols
- Review SI analysis of PCIe 5.0 implementation on PICMG COM-HPC Carrier/Server Module
- Solve typical SI challenges for embedded applications using selected Samtec products. These include:
- The SEARAY™ SEAF & SEAM connectors, which offer high-speed performance of up to 56 Gbps and protect against electrostatic discharge (ESD), tested at 5, 10, and 15 kV.
- The APF6 & APM6 AcceleRate® High-Performance Terminals, which feature 112 Gbps PAM4 extreme performance and are PCIe® Gen 5 compatible.
- The NovaRay® Extreme Performance High-Density Arrays, which consume 40% less space compared to traditional arrays with the same data throughput. The arrays also offer extremely low crosstalk, as well as an aggregate data rate of 4.0 Tbps.
- The PCI Express Edge Card Sockets, which come in four different designs and support 1, 4, 8, and 16 PCI Express links.
- The COM-HPC™ Interconnect Solutions, which provide ultra-high-speed performance and extended connectivity with limitless scalability.
- The AcceleRate® Slim Body Direct Attach Cable Assembly, which includes the ARF6 vertical slim socket and the ARF6-RA right-angle slim socket, complete with rugged metal latching and shielding.
The webinar will be hosted by Mark Patrick, Head of Technical Marketing, EMEA at Mouser Electronics and will feature Matthew Burns, Global Director Technical Marketing at Samtec, as a guest speaker.
To register for this free webinar, visit https://emea.info.mouser.com/webinar-samtec-singnalintegrity-emea-lp/.
To learn more about Samtec, visit https://www.mouser.com/manufacturer/samtec/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser är en ledande auktoriserad distributör av elektroniska komponenter och produkter för industriell automation. Med fler än 6,8 miljoner produkter från över 1 200 varumärken erbjuder vi det bredaste urvalet av produkter i lager. Vår verksamhet inom elektroniska komponenter vänder sig till konstruktörer och inköpare med nya produktlanseringar inom halvledare, passiva komponenter, kontaktdon och relaterad elektronikteknik. Vår verksamhet inom industriell automation hjälper företag att utforma, bygga och underhålla sin tillverkningsutrustning och drift med lösningar som omfattar de senaste sensorerna, kontrollpanelerna, PLC:erna och motorstyrningarna – där allt finns i lager för omedelbar leverans.
Mouser erbjuder förstklassig kundservice med 28 kontor världen över som erbjuder support på ditt språk, i din valuta och i din tidszon. Vi levererar dagligen produkter till fler än 650 000 kunder i 223 länder och territorier från våra toppmoderna distributionsanläggningar på över 1,5 miljoner kvadratfot i storstadsområdet Dallas i Texas. Mer information finns på https://www.mouser.com.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.