Mouser Electronics Supports Advanced Underwater Harvester Project for UK Seagrass Restoration
13 November 2025 – Mouser Electronics, Inc., the authorised global distributor with the newest electronic components and industrial automation products, announces its latest initiative supporting UK seagrass conservation. In a project led by marine conservation experts, components supplied by Mouser have enabled the development of an innovative underwater harvester prototype that aims to accelerate seagrass seed collection, making large-scale restoration faster, safer, and more precise.
Seagrass: Vital yet Vanishing
Seagrass meadows are among the most valuable coastal ecosystems on Earth. They stabilise sediments and reduce wave energy, protecting coastlines from erosion and storm surges, while improving water quality by filtering pollutants and excess nutrients. These underwater biomes also serve as biodiversity hotspots, providing habitat and nursery grounds for fish, invertebrates, and endangered species that underpin global food security and local fisheries.
Beyond their immediate ecological benefits, seagrass meadows act as a powerful carbon sink, storing carbon up to 35 times more efficiently than tropical rainforests and accounting for around 10% of the ocean’s carbon, despite covering only 0.2% of the seabed[1]. However, researchers have found that at least 44% of the UK’s seagrass has been lost since 1936, with up to 92% likely to have vanished over longer time spans[2] – underscoring the urgency of conservation and restoration.
About the Project
One of the greatest challenges in seagrass restoration is that manual seed collection is slow and costly. This project brings together engineers Sam Rogers and Edwin Towler from Tandem Ventures, with Mouser Electronics, to develop a prototype for Project Seagrass, a global marine conservation organisation. This pioneering system aims to collect seeds up to 100 times faster than manual methods, opening the door for larger-scale seagrass restoration worldwide.
Mouser supplied the project with a wide range of components, including the Analog Devices Inc. (ADI) EVAL-ADXL362 Evaluation Board, Espressif Systems ESP32-S3-WROOM-1/1U Wireless Module, STMicroelectronics LSM6DSOTR 6-axis inertial measurement unit (IMU), and connectors from JST and Hirose Electronics. The performance of these components ensures that the project’s requirements for high-precision sensing, data processing, and reliable operation in challenging underwater environments are fulfilled, helping to advance seagrass conservation efforts.
“We are very proud to be part of this endeavour, supporting the restoration of ‘underwater rainforest’ environments. It’s exciting to see technology helping conservation in such a tangible way,” comments Mark Patrick, Director of Technical Content, Mouser Electronics. “Mouser strives to demonstrate how innovation can accelerate ecological restoration without compromising scientific integrity or operational safety.”
This initiative represents an example of Mouser’s focus on corporate social responsibility and follows on from Mouser’s previous sustainability projects, including the whale research and conservation program and the planting of thousands of trees across the United States and Europe, one for every ADI order in 2023.
To see the underwater harvester in action and learn more about this pioneering seagrass restoration project, visit https://www.youtube.com/watch?v=mg3o02olguc.
[1] https://www.unep.org/news-and-stories/story/seagrass-secret-wepon-fight-against-global-heating
[2] https://www.frontiersin.org/journals/plant-science/articles/10.3389/fpls.2021.629962/full
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.