Mouser Electronics and Analog Devices Present Webinar on Using Radar and Sensor Fusion to Elevate Robotic Solutions

För omedelbar lansering

Anslut till oss


7 October 2024Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, has partnered with Analog Devices, Inc. (ADI) to offer the engineering community a new webinar called ‘Optimising Robotics with Radar and Sensor Fusion Technologies’. The free webinar will take place on 29 October 2024 at 17:00 CET.

With the increasing use of robotics across various industries, solutions for precise perception and movement have become ever more important—especially if robots are to operate safely alongside humans. Achieving this requires a wide range of perception sensors, enabling control electronics to evaluate a situation accurately and to achieve safe and efficient operation. Radar technology is a key element of robot perception sensing, providing object detection regardless of light levels, precise distance measurement, and accurate mapping of the surrounding environment.

This webinar will provide valuable insight to improve the performance, safety, and efficiency of robotic radar systems, including strategies for seamless sensor fusion. It will also explore the role of Gigabit Multimedia Serial Link (GMSL™) technology in ensuring fast data transmission, including information on how converting GMSL signals to Ethernet can enhance communication and network integration. Enhancing radar and sensor fusion in robotics can maximise the performance, safety, and efficiency of robotic systems, allowing them to effectively cater to the demands of modern industry.

By attending this webinar, participants will discover more about:

  • The latest innovations in radar systems (24-77GHz) and GMSL to Ethernet boards for robotics and industrial automation.
  • Practical applications and product advancements for enhancing industrial processes.
  • Developing comprehensive solutions that leverage featured products, including:
    • AD-GMSL2ETH-SL edge compute platform, which supports the integration of up to eight GMSL camera interfaces, enabling highly accurate machine vision and real-time sensor fusion in autonomous robots and vehicle applications.
    • ADTF3175 1-megapixel time-of-flight (ToF) module, which is a CMOS indirect ToF sensor designed for high-resolution 3D depth sensing and vision systems.
    • TMC2210STEPSTICK evaluation board, which is a convenient solution that allows for streamlined development of ADI’s TMC2210 stepper motor driver ICs.
    • ADF5902 24GHz radar transmitter, which is a compact monolithic microwave integrated circuit (MMIC) featuring a programmable grid array (PGA) and dual transmitter channels.
    • TMCM-1617-GRIP-REF reference design, which is a comprehensive solution featuring open-source hardware reference design and a wide range of I/O options to expedite the development process.
    • MAX96717/F/R DPHY evaluation kits, which enable engineers to easily evaluate ADI’s MAX96717 high-bandwidth GMSL serializer.

The webinar will be hosted by Mark Patrick, Director Technical Content EMEA, Mouser Electronics and will feature Anders Frederiksen, Senior Strategic Marketing Manager – Robotics and Emerging Technologies, ADI, and Rajan Sharma Senior Strategic Marketing Manager – Robotics and Emerging Technologies, ADI as guest speakers.

To register to stream the webinar live or to receive a recording of the webinar once it is available, visit https://emea.info.mouser.com/webinar-adi-robotics-emea/.

To learn more about ADI, visit https://www.mouser.com/manufacturer/analog-devices/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För pressförfrågningar, kontakta:
Janice Fenton
Direktör för B2B-kundansvar med ansvar för originalitetsverifiering
+44 (0) 7984 077330
För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833