Mouser Expands Global Distribution Agreement with Eaton Corporation to Include Eaton Electrical

För omedelbar lansering

Anslut till oss


January 13, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, today announces an expanded global distribution agreement with Eaton to include its electrical distribution and control portfolio. Eaton is an intelligent power management company with deep regional application expertise in power distribution and circuit protection; power quality, backup power and energy storage; control and automation; life safety and security; structural solutions; and harsh and hazardous environment solutions. With almost 125,000 products from Eaton's divisions available to order, including over 15,000 in stock, Mouser offers a wide portfolio of Eaton solutions for use in aerospace, automotive, data center, transportation and industrial applications.

The FAZ-series UL 489 circuit breakers and UL 1077 supplementary protectors from Eaton are miniature, DIN-mounted devices that offer optimum and efficient protection for personnel, installations and plants. The UL 489 circuit breakers offer up to 63 A current rating and are designed for use in branch service applications such as UPS, motor control circuits, PLC I/O points, HVAC systems and more. The UL 1077 supplementary protectors are designed for use in control panel applications such as control circuits, lighting, and business equipment.

The XLHV supercapacitors from Eaton Electronics Division are high reliability, high power, ultra-high capacitance energy storage devices. These devices feature an electric double-layer capacitor (EDLC) construction, allowing for enhanced application flexibility for backup power, pulse power, and hybrid power systems.

The UTSX circular connectors from Eaton / SOURIAU are UV/corrosion-resistant and resistant to shock, making them ideal for harsh environments. These connectors are built with a unique design of interchangeable contacts that simplifies the supply chain and maintains the same cabling process across all ranges. The typical applications include off-road machinery, instrumentation, outdoor solar, irrigation systems, wind management, and water management.

The AS85049/88/89/90 EMI/RFI composite backshells from Eaton / SUNBANK are self-locking, highly reliable, and able to withstand high vibrations. These backshells offer signal integrity by facilitating shield attachment. Typical applications include aviation, ground army, military marine, military aircraft, and ground transportation.

Eaton has honored Mouser with their 2023 Electronics Division Distributor Partnership Award in the Americas. Mouser also received the Distributor Engagement Award from Eaton for 2019.

To learn more about the Eaton power, protection and connection solutions available from Mouser, visit https://www.mouser.com/manufacturer/eaton/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About Eaton

2026 - Eaton's electrical business is a global leader with deep regional application expertise in power distribution and circuit protection; power quality, backup power and energy storage; control and automation; life safety and security; structural solutions; and harsh and hazardous environment solutions. Through end-to-end services, channels and an integrated digital platform & insights, Eaton is powering what matters across industries and around the world, helping customers solve their most critical electrical power management challenges.

Eaton is an intelligent power management company dedicated to protecting the environment and improving the quality of life for people everywhere. They make products for the data center, utility, industrial, commercial, machine building, residential, aerospace and mobility markets. They are guided by their commitment to do business right, to operate sustainably and to help customers manage power ─ today and well into the future. By capitalizing on the global growth trends of electrification and digitalization, Eaton is accelerating the planet's transition to renewable energy sources, helping to solve the world's most urgent power management challenges, and building a more sustainable society for people today and generations to come.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764