Mouser-Backed DS PENSKE Formula E Racing Team Celebrates a Pole Position and a Stunning 1st and 2nd Place Double Podium in Shanghai

För omedelbar lansering

Anslut till oss


June 2, 2025 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, congratulates the DS PENSKE Formula E racing team for scoring an unprecedented P1-P2 finish in round 10 of the ABB FIA Formula E World Championship at the Shanghai, China, International Circuit.

Team driver Maximilian Günther led the charge, starting the race in Pole 1 after topping the timesheets in the qualifying rounds. Günther led the pack through much of the race, converting his initial position into his second victory of the season with a respectable seven-second lead. Meanwhile, teammate Jean-Éric Vergne cunningly conserved his energy until the last lap, then pulled off several overtakes to score second place, propelling the team up to third place in the Team Championship. Vergne also crossed the finish line in 5th position in round 11, contributing valuable points to the team's tally.

"Congratulations to Max, Jean-Éric, and the entire DS PENSKE team on their incredible performance and strategy this weekend," said Todd McAtee, Mouser Senior Vice President of Business Development Americas. "Jean-Éric's last-minute overtakes were a thrilling highlight of the weekend, and the team continues to position themselves as a contender in the season championship. Great job, everyone!"

Mouser is supporting the DS PENSKE team for the globe-trekking 2024/2025 season in collaboration with TTI, Inc., and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.

Formula E cars are powered solely by electricity and represent a vision for the future of the motorsports industry, serving as a framework for research and development around zero-emission motoring. Racing is all about speed and endurance, and racing partnerships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

To learn more about the Mouser-backed DS PENSKE Formula E team and view the ABB FIA Formula E World Championship Racing Season 11 schedule, visit https://www.mouser.com/formula-e/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764