Mouser Electronics Stocking Newest Connectivity Solutions from Digi International Inc.

För omedelbar lansering

Anslut till oss


March 25, 2024Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is an authorized global distributor for Digi International Inc., a global leader in Machine-to-Machine (M2M) and Internet of Things (IoT) connectivity products and services. Mouser's longstanding business partnership with Digi supports Mouser customers in the development of solutions for Internet of Things (IoT), medical, industrial, and transportation applications, among others. 

Mouser stocks more than 600 different products from Digi, in addition to more than 1,000 part numbers available to order. The Digi ConnectCore® 93 system-on-module (SoM) provides reliable wireless communication, maximum power efficiency, and enhanced security for embedded devices. Key features include Wi-Fi® 6 and Bluetooth® 5.2 connectivity, Arm® Cortex®-A55 cores, and an AI/ML Arm Ethos U65 neural processing unit.

The new Digi XBee® XR 868 RF modules are designed for long-range connectivity applications. The XBee XR 868 radio frequency modules operate in the 863 to 870 MHz frequency range and support point-to-point and mesh networking protocols. Listen Before Talk (LBT) and Adaptive Frequency Agility (AFA) allow the system to assess and adapt to the radio environment, reducing interference.

Mouser also stocks the Digi XBee® 3 Global LTE Cat 1 embedded modem, which allows OEMs to incorporate cellular connectivity easily into their device designs. The embedded modem is ideal for a range of IoT applications that require moderate bandwidth and low-cost solutions. The modem is supported by the Digi XBee® 3 Global GNSS LTE CAT 1 development kit.

The Digi XBee® 3 Global LTE-M/NB-IoT smart modem offers quick time to market, wireless connectivity, and easy-to-add functionality. The XBee 3 Global LTE modules include multiple power-saving features, making them a suitable choice for IoT applications that require low power consumption and long battery life. Digi XCTU® software tools simplify setup, configuration, and testing.  

Mouser has been an official distributor of Digi products since 2005 and was named the New Product Introduction (NPI) Distributor of the Year by Digi in 2018, 2020, and 2021. To learn more about Digi products available from Mouser Electronics, visit https://www.mouser.com/manufacturer/digi-international/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About Digi

2026 - Digi International is a global technology leader empowering enterprises to build, connect, and manage the critical systems that drive their businesses. Through an integrated portfolio of managed services, intelligent software, secure connectivity, and resilient edge solutions, Digi helps enterprises monitor, update, and control assets in real time, strengthen compliance, streamline workflows, and keep distributed operations running without interruption. Since 1985, Digi has enabled organizations worldwide to modernize operations and confidently connect millions of devices.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764