Digi ConnectCore 93 System-On-Module, Now Available at Mouser, Supports Longevity and Scalability for Industrial IoT Applications

Nya produktlanseringar

Anslut till oss


Learn more about the ConnectCore 93 SOM

December 5, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the ConnectCore® 93 system-on-module (SOM) from Digi. Based on the industrial NXP Semiconductors i.MX 93 applications processor, the ConnectCore 93 SOM is designed for a wide range of Internet of Things (IoT) devices for medical, industrial, energy, and transportation. The new SOM is an ideal choice for automation, human-machine interfaces, equipment monitoring, edge computing, and machine learning applications.

The Digi ConnectCore 93 SOM, now available at Mouser, features up to two Arm® Cortex®-A55 cores, while a Cortex-M33 core, AI/ML Arm Ethos U65 NPU and NXP PMIC ensure maximum power efficiency. The SOM features pre-certified dual-band 802.11ax Wi-Fi 6 and Bluetooth® 5.3 connectivity, as well as seamless cellular modem and Digi XBee® integration. Housed in a surface-mount, 40 mm x 45 mm form factor, the ConnectCore 93 SOM is designed to deliver industrial reliability for embedded devices. The new SOM also offers exceptional security and privacy with Digi TrustFence®, a fully integrated device security framework that simplifies the process of securing connected devices. The ConnectCore 93 SOM supports an industrial operating temperature range of -40 °C to +85 °C, in addition to product lifecycles of 10+ years for embedded devices. This SOM is designed for industrial reliability and 10+ year product lifecycles of embedded devices. The Digi SMTplus® surface-mount form factor provides simplified design integration, efficiency and reliability.

The ConnectCore 93 SOM is supported by the ConnectCore 93 development kit. This comprehensive demonstration platform includes a development board and an i.MX 93 dual-core, NPU, 8 GBytes eMMC, and 1 GByte LPDDR4 wireless SOM. The development kit also includes reference designs and online documentation, allowing designers to quickly prototype and scale industrial IoT applications.

To learn more about the ConnectCore 93 SOM, visit https://www.mouser.com/new/digi-international/digi-connectcore-93-soms/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Digi

2026 - Digi International (Digi) is a leading global provider of mission-critical machine-to-machine (M2M) and Internet of Things (IoT) connectivity products and services. The company helps its customers create next-generation connected products and deploy and manage critical communications infrastructures. Founded in 1985, Digi has helped customers connect over 100 million things, and growing.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764