Mouser Electronics Signs Distribution Agreement with BreadBoard Mates to Deliver Development Display Technologies

För omedelbar lansering

Anslut till oss


November 30, 2022 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, announces a new global distribution agreement with Breadboard Mates, a leading supplier of micro-LCD-displays for breadboard and electrical development projects. Breadboard Mates’ Tiny Intelligent Modular Instrument (TIMI) hardware and Integrated Development Environment (IDE) software products are designed to replace and simulate component readouts and meters that demand extensive hardware resources for breadboard or electronic development projects.

Mouser is now stocking the latest BreadBoard Mates products, including the TIMI-96 display development module. The TIMI-96 incorporates hundreds of built-in widgets, allowing design engineers to streamline development projects using fewer components at lower cost. The TIMI-96 display development module is a 160 × 80, 0.96” TFT LCD module featuring a 4D Labs PIXXI-28 graphics processor for stand-alone, host-driven interfaced, PC-tethered, and educational applications.

The TED-96 display module is the OEM version of the TIMI-96 module, designed for product integration where the TIMI-96 may not be suitable. The TED-96 is a 0.96” TFT In-Plane Switching (IPS) LCD module also driven by the 4D Labs PIXXI-28 graphics processor. The module includes both castellated and through-hole pads at each end to allow for different mounting options. Various interfaces arm the TED-96 with resources to be either a stand-alone controller, a host-driven secondary device, or a tethered instrument while being able to interface with and power external devices. For larger displays, Mouser offers the BreadBoard Mates TIMI-130 — a unique breadboard-compatible display development module with a 1.3” TFT IPS LCD (40 × 240) display. The TIMI-130 features a unique MatesBus interface, which is simple to use in breadboard applications, adapters, or directly into products. The main TIMI-130 interface is a 3.3 V level asynchronous serial UART featuring three GPIOs that can be used as digital or analog inputs, digital outputs, master I²C communication, or PWM audio output.

The TIMI-MB display development module provides a simple interface display solution for boards and modules that include MikroBUS sockets. The TIMI-MB module is a 0.96” TFT LCD with a five-pin programming header that programs its processor using the Mates Programmer, a selection switch that alternates between programming modes or connection to the MikroBUS host. The TIMI-MB module is a flexible design aid for demanding hardware resources for breadboard and electronic development projects.

To learn more about the BreadBoard Mates products now available from Mouser Electronics, visit https://www.mouser.com/manufacturer/breadboard-mates/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About Breadboard Mates

2026 - Breadboard Mates was established in October 2020 to bring breadboard-friendly products to the market, significantly reducing the time and components required to develop and experiment with electronics. From hobbyist to engineering professional, Breadboard Mates cutting edge products can be utilized for seamless development with the help of the integrated products like TIMI (Tiny Intelligent Modular Instrument) and the Mates Studio software development tool. Mates Studio is unlike any other, offering four different programming methods with a library of hundreds of pre-designed pages and widgets. The result is an unprecedented increase in development speed for stand-alone, host driven or PC testing applications.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764