Mouser Now Shipping Banner Engineering Asset Monitoring Gateways with SNAP ID for Industrial Applications
November 13, 2023 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the AMG-SNAP-ID asset monitoring gateways with SNAP ID from Banner Engineering. Utilizing data from up to 20 connected sensors, these asset monitoring gateways help facilitate decisions about industrial asset management and maintenance for almost any facility asset, such as conveyor systems, industrial fans, pumps, electric motors, compressed air systems, and dust-collection units.
The Banner Engineering AMG-SNAP-ID asset monitoring gateways are specifically designed for condition monitoring for predictive maintenance. The gateway and the optional Cloud Data Services platform allow users to access, store, and export critical data collected by connected sensors. Using actionable device data, it is easy to identify trends, predict maintenance requirements, avoid costly equipment failures, and prevent unplanned downtime.
The AMG-SNAP-ID gateways feature a user-friendly, no-code setup and are preconfigured to easily connect with a wide variety of compatible SNAP ID wired sensors right out of the box for measuring vibration, differential pressure, temperature, humidity, tank level and more. Ethernet or cellular connectivity can be easily configured through the display.
With the AMG-SNAP-ID asset monitoring gateways, critical system information is easily viewed locally via the onboard touchscreen display or remotely using the Banner Cloud Data Services (CDS) platform, which provides access to the data in customizable online dashboards. Banner CDS lets users set condition-based alerts from the cloud using multiple metrics of event severity and duration of time. These provide remote users with emails or SMS, based on parameters specified in the cloud. Building a dashboard in Banner CDS is easy. Drag-and-drop widgets and the ability to load images to the dashboard let users create exactly what they need to visualize their operation.
To learn more, visit https://www.mouser.com/new/banner-engineering/banner-amg-hardware/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
2026 - Banner Engineering designs and manufactures industrial automation products, including sensors, smart IIoT and industrial wireless technologies, LED lights and indicators, measurement devices, machine safety equipment, barcode scanners, and machine vision. These solutions help make many of the things people use every day, from food and medicine to cars and electronics. A high-quality, reliable Banner product is installed somewhere around the world every two seconds. Headquartered in Minneapolis since 1966, Banner is an industry leader with more than 10,000 products, operations on five continents, and a worldwide team of more than 5,500 employees and partners. The company's dedication to innovation and personable service makes Banner a trusted source of smart automation technologies to customers around the globe.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.