Mouser Electronics Signs Global Agreement to Distribute ATP Electronics Storage and Memory Solutions

För omedelbar lansering

Anslut till oss


June 29, 2022Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, announces a global distribution agreement with ATP Electronics, the global leader in specialized storage and memory solutions. According to the agreement, Mouser now offers customers ATP Electronics’ memory cards, SSDs, and managed NAND devices for industrial and automotive applications.

ATP’s industrial solid state drives (SSDs) and modules deliver dependable performance, efficient responsiveness, and long usage life to accomplish mission-critical tasks. Sturdy and built to withstand rigorous operating environments, ATP SSDs are available in form factors such as 2.5” SSDs, M.2 embedded modules, mSATA, eUSB, and industrial USB drives for enterprise and industrial applications. The devices support high-speed interfaces such as SATA 6 Gb/s and the latest NVMe™ protocol on a PCIe® 3.0 x4 interface for reliable, blazing-fast, and future-ready performance.

The e.MMC v5.1 embedded flash storage solution is an extremely durable storage solution for applications such as surveillance, test and measurement, drones, and medical devices. The e.MMC solution combines NAND flash memory, a fast MultiMedia Card (MMC) interface, and a sophisticated flash controller. The high-performance devices are compliant with AEC-Q100 Grade 2, AEC-Q100 Grade 3, and JEDEC e.MMC v5.1.

ATP Electronics’ DDR4 DRAM solutions offer fast performance with impressive power savings, combining a 3200 megatransfers per second (MT/s) data transfer rate with just 1.2 V of power consumption. The DDR4 solutions support the increased bandwidth needed to scale online traffic, providing an ideal solution for applications including networking systems, telecommunication, gaming, and cloud servers.

The industrial-grade SD/SDHC/SDXC and microSD cards from ATP Electronics offer ideal storage for automotive and industrial applications, including automotive in-vehicle infotainment systems, test and measurement devices, and navigation products. The rugged cards are designed to deliver extensive longevity and feature power failure protection for increased reliability.

To learn more, visit https://www.mouser.com/manufacturer/atp-electronics/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About ATP Electronics

2026 - ATP Electronics (“ATP”) has dedicated 30 years of manufacturing excellence as the premier provider of memory and NAND flash storage products for rigorous embedded/industrial/automotive applications. As the “Global Leader in Specialized Storage and Memory Solutions,” ATP is known for its expertise in thermal and high-endurance solutions. ATP is committed to delivering add-on value, differentiation and best TCO for customers. A true manufacturer, ATP manages every stage of the manufacturing process to ensure quality and product longevity. ATP upholds the highest standards of corporate social responsibility by ensuring sustainable value for workers, the environment, and business throughout the global supply chain.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764