Mouser Electronics Partners with ATI Industrial Automation with Global Distribution Agreement
November 11, 2025 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announces a global distribution agreement with ATI Industrial Automation. ATI Industrial Automation is a leading engineering-based developer of robotic accessories and robot arm tooling, including automatic tool changers, multi-axis force/torque sensing systems, material removal tools, robotic collision sensors, and compliance devices.
The ATI Industrial Automation Axia multi-axis force/torque (F/T) sensor system, now available from Mouser, measures all six components of force and torque. Electronics and communication options are common across all Axia models to simplify integration and high-volume deployment. Force/Torque sensors are used throughout the industry for product testing, robotic assembly, pick and place, and automation. The Axia90-M50, Axia130-M125, and Axia130-M300 offer seamless ISO-standard mechanical integration, IP67 environmental protection, and 50Nm, 125Nm, and 300Nm load ratings. The Axia130 sensors also include a large through-hole for easy routing of cables and other utilities through the center of the sensor.
ATI Industrial Automation robotic tool changers provide the flexibility to automatically change robotic arm end-effectors or other peripheral tooling. The end-effectors feature two mating parts, a Master-side and a Tool-side, that have been designed to lock or couple together automatically, carry a payload, and have the ability to pass utilities such as electrical signals, pneumatic, or water. The Master side of the Tool Changer mounts to a robot, CNC machine, or other structure. The Tool-side of the tool changer mounts to tooling, such as grippers, welders, or deburring tools.
The QC-76 robotic tool changers feature a lightweight design with high strength. The QC-76 series features five connections for passing air or vacuum through the tool changer, and two connections to supply pneumatic pressure for coupling and uncoupling. The QC-76 series has a 100 kg suggested payload limit.
The QC-7 series changers are lightweight and durable, offering a variety of configuration options. This series has a 16 kg suggested payload limit. Other features include an optional tool stand hook for convenient storage during tool change, and a slotted tool for light-duty, economical tool storage.
The QC-29 robotic tool changers bring the powerful and rugged technology of ATI heavy-duty tool changers to the 25kg to 35kg payload class. The QC-29 series changers are designed to mount directly to 40 mm and 50 mm robot wrists. The QC-29 also includes in-body lock/unlock sensing and a Fail-Safe locking mechanism.
To learn more about ATI Industrial Automation, visit https://www.mouser.com/manufacturer/ati-industrial-automation/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
2026 - ATI Industrial Automation is an engineering-based developer of robotic accessories and robot arm tooling, including automatic tool changers, multi-axis force/torque sensing systems, utility couplers, manual tool changers, and robotic collision sensors. Since 1989, this company has developed state-of-the-art end-effector products and solutions that improve robotic productivity.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.