Mouser Electronics Unveils Edge Computing Solutions for Any Engineering Challenge

För omedelbar lansering

Anslut till oss


August 21, 2023Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is serving engineers with trusted resources for the evolving challenges and opportunities of Edge Computing. Their digital library is packed with informative and engaging content that supports professionals with in-depth articles tailored to a broad spectrum of needs like AI on the Edge and Edge Cybersecurity. In two of Mouser's recent eBooks, Bringing Intelligence to the Edge and Intelligence at the Edge, leading experts from Mouser, Renesas and STMicroelectronics explore using artificial intelligence (AI) and machine learning (ML) in edge computing. Designers will find cutting-edge solutions, high-quality products and enhanced models within Mouser's dozens of articles, videos and blogs.

With the growing popularity of edge computing in various professional and consumer systems, it is crucial for engineers to have easy access to relevant and practical solutions. Mouser's Edge Computing content hub provides a carefully curated selection of resources that keep engineers up to date with the latest edge computing developments. Mouser offers this comprehensive range of content designed to help engineers make informed decisions and implement effective solutions.

Mouser's Edge Computing resource page is an integrated service center where customers can find the latest products and industry information quickly and easily – all in one place. Additionally, Mouser stocks the industry's widest selection of semiconductors and electronic components, including the following solutions for edge computing applications:

  • NXP Semiconductors SLN-VIZNAS-IOT Solution for Face Recognition is an EdgeReady development kit for secure face recognition based on the i.MX RT106F Crossover Processor. It features liveness detection, fully integrated turnkey software, and IR and RGB cameras. This i.MX RT106F MCU-based solution is suitable for a variety of smart home applications, smart industrial devices, security, and more.
  • Semtech LoRa Edge™ LR1120 Wi-Fi/GNSS Scanner + LoRa® is a low-power, long-range transceiver that leverages Semtech's LoRa Cloud™ services. It complies with the physical layer requirements of the LoRaWAN® standard specification while also being able to meet various application requirements. It's best used in intercontinental logistics, multi-regional inventory management, asset loss and theft prevention, and more.
  • STMicroelectronics B-U585I-IOT02A Discovery Kit enables a wide range of applications by exploiting low-power communication, multiway sensing, and direct connection to cloud servers. With 2Mbytes of Flash memory, 786Kbytes of SRAM, and smart peripheral resources, the kit provides unlimited expansion capabilities with a wide choice of specialized add-on boards. It supports a range of wearable or sensor applications in fitness, metering, industrial, or medical, with state-of-the-art energy efficiency and higher security.
  • Advantech ESRP-PCS-ADAM6 Intelligent I/O Gateways has a built-in WISE-EdgeLink that supports over 200 drivers, enabling efficient real-time data transmission from the edge to the cloud. The ADAM-6 facilitates data transmission between edge devices and the cloud and is ideal for factory management and energy monitoring. It can perform multiple tasks at the edge and comes with Linux OS installed with its integrated design.
  • Terasic Technologies FPGA Cloud Connectivity Kit, available to order at Mouser, is certified with key cloud service providers (CSPs) and comes with open-source design examples that support new users through the process of connecting an FPGA-based edge device to the cloud for the first time. It's based on the Terasic DE10-Nano Kit and adds Wi-Fi® and Bluetooth® wireless communication while featuring an ambient light sensor, humidity and temperature sensor, Bluetooth SPP, and more.

For the latest on solutions for edge computing, visit https://resources.mouser.com/edge-computing/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För mer information, kontakta:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
Vid pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804 7764