Mouser Connects Engineers to the Future of EV/HEV Technology with New Comprehensive Resource Hub

För omedelbar lansering

Anslut till oss


June 27, 2024Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, explores the latest developments, advancements and challenges in electric and hybrid vehicle technology through its extensive EV/HEV resource hub. Staying ahead in this rapidly evolving industry is crucial for engineers and innovators. With advancing technologies like bi-directional charging and vehicle autonomy entering the market, it's more important than ever to stay up to speed. Mouser's EV/HEV resource hub offers a wealth of engaging content, including eBooks, blogs, articles, products, and more, all designed to keep engineers at the forefront of these technological advancements.

Across the globe, electric vehicles (EV) and hybrid electric vehicles (HEV) are changing not just the way people drive but also the way people live. Electric infrastructure is advancing with the use of emerging technologies, such as liquid-cooled HPC connectors, while still maintaining the latest industry standards and lowering maintenance costs. This development empowers the future of eMobility, as discussed in Mouser's interactive content series Electrifying the Future of eMobility, exploring how current renewable energy sources and evolving technologies like hydrogen electrolysis are driving toward a net-zero future.

The EV/HEV technology content hub offers engineers easy access to resources from Mouser's technical team and leading manufacturers. In a recent eBook with TE Connectivity, EV and Connected Transportation, industry experts explain the tandem movement of e-mobility and connected travel via new standards and the use of the V2X ecosystem to make more efficient, accurate, and safer roads for vehicles. The benefits and challenges of designing solutions for the future of transportation are discussed in depth, including the differences in wireless charging and battery swapping in green freight technology.

Mouser stocks the industry's widest selection of semiconductors and electronic components, including the following solutions from top manufacturers for EV/ HEV applications:

  • KM3x 32-bit microcontrollers from NXP Semiconductors are precision metrology MCUs with segment LCDs and are based on an Arm® Cortex®-M0+ core. They provide a low-cost and highly integrated solution for electricity meters that require powerful 32-bit processing capability, precision-analog, security, and HMI functionality. The KM3x MCUs provide security through tamper detection with time stamping for various EV applications.
  • The MX150 mid-voltage connectors from Molex are designed to meet the growing demand in the automotive industry for 48V electrical systems. The connectors offer a pre-assembled terminal position assurance housing and one-piece, 3.50mm-pitch housing for applications in automotive, commercial vehicles, power, and more.
  • The AEKD-STEREOAVAS integrated stereo AVAS kit by STMicroelectronics provides a demonstration and prototyping platform for an acoustic vehicle alerting system (AVAS). An AVAS is designed to emit vehicle warning sounds and alert pedestrians to the presence of electric drive vehicles.
  • The BQ79718-Q1 automotive 18S battery monitor by Texas Instruments provides high-accuracy cell-voltage measurements for up to 18 battery modules in high-voltage battery management systems (BMS) for HEVs and EVs.
  • The 1200V CoolSiC™ M1H modules from Infineon Technologies deliver superior gate-oxide reliability, which is allowed by its state-of-the-art trench design. With the ability to tailor the modules for different application needs, they provide various benefits of higher frequency operation to reduce system and operational costs for fast EV charging or solar energy systems.

To browse Mouser's EV/HEV resources, visit https://resources.mouser.com/ev-hev/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764