AMobile Solutions SoM-SD520 and SoM-SD720 SoMs, Now Available from Mouser, Enable AI and Machine Vision Applications

Nya produktlanseringar

Anslut till oss


Learn more about the SoM-SD520 and SoM-SD720 SoMs
Learn more about the SoM-SD520 and SoM-SD720 SoMs

March 10, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new SoM-SD520 and SoM-SD720 System-on-Modules (SoMs) from AMobile Solutions. These production-ready SoMs are fully optimized for both transformer-based language generation and convolutional neural network (CNN)-based vision analytics. With support for running popular large language models (LLMs), the platform provides powerful AI acceleration for a wide range of AI, human-machine interface (HMI), smart home, smart retail, industrial, and commercial IoT applications.

The SoM-SD520 and SoM-SD720 SoMs are based on the Genio 520 and 720 high-performance Gen-AI IoT system-on-chips (SoCs) from MediaTek. The Genio 520 and 720 AI Platforms deliver up to 10 TOPS with a built-in MediaTek 8th-generation Neural Processing Unit (NPU) and integrate an octa-core CPU with two Arm® Cortex®-A78 processors and six Cortex-A55 processors to optimize performance and power efficiency.

The SoM-SD520 and SoM-SD720 support up to two internal ISPs and six FHD MIPI virtual channels, offer multi-display output (eDP 4K60, DP 5K60), and feature extensive I/O interfaces, making them ideal for multi-camera AI-powered home surveillance systems, in-store AI camera systems, visual defect detection, and interactive signage.

Also available from Mouser, the Genio_520_EVK and Genio_720_EVK evaluation kits are easy-to-use, full-featured prototyping and development platforms for the Genio 520 and 720 chipsets. Both evaluation kits include a main board, camera boards, a 7" LCD with touch display, a pre-installed Wi-Fi® 6 / Bluetooth® 5.2 module, a Wi-Fi antenna, and the required cables. The evaluation kits serve as an accelerator for engineering teams, enhancing development cycles while maintaining high standards of quality and performance, reducing development time, minimizing project risks, and speeding time-to-market.

To learn more, visit https://www.mouser.com/new/amobile-solutions/amobile-som-sd520-sd720-arm-system-on-modules/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About AMobile Solutions

2026 - AMobile Solutions is a joint investment by MediaTek and ARBOR Technology. The company aims to create next-generation industrial-grade handheld devices and AI machine vision integration solutions. As a leader in rugged handheld devices and tablets, AMobile has established itself as a global brand marketing products in dozens of countries. The company is an expert in rugged communication devices and AIoT machine vision integration. It offers solid handheld communication devices, rugged tablets, machine vision processing, and more. With AMobile's all-in-one production model and as a joint venture of MediaTek, the company has access to the latest chip technology, enabling it to develop and create versatile handheld products for industries such as warehousing, automotive, retail, public safety, healthcare, and military applications. Through specialized industrial design, modular hardware manufacturing processes, and a dedicated software team, AMobile creates products tailored to specific industry applications.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764