Mouser Electronics Delivers Expert Perspectives on Motor Control in New eBook from Analog Devices
May 13, 2025 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announces a new eBook in collaboration with Analog Devices, Inc. (ADI), exploring the latest trends and challenges in motor control. From industrial robots and factory automation systems to medical devices, consumer electronics, and electric vehicles (EVs), motors drive the machinery that powers our modern world. In 14 Experts Discuss Motor Control in Modern Applications, engineers from ADI and other technology companies offer their perspectives on how ADI is helping meet the growing demands for intelligent, high-performance motor solutions. ADI is a world leader in motor control and provides customers with a broad portfolio of solutions, many of which are highlighted in the eBook.
The ADI TMC8100 universal encoder bus controller, available from Mouser, acts as a peripheral interface block to deliver the extracted and adjusted encoder position information to a motor control circuit's microcontroller or motion controller over SPI or UART. The device offers a high degree of flexibility for current protocol implementations, customization, and future protocol extensions.
The TMC9660 combines a smart gate driver and a high-performance motion and servo controller. The device also integrates motion position feedback interfaces, analog-to-digital converters (ADC), a powerful and flexible power management unit (PMU) and programmable low-dropout (LDO) regulators. For control and communication with an external processor through SPI or UART, a preprogrammed 32-bit microcontroller is embedded. Integrating the motor drive and controller of the TMC9660 simplifies the design and improves energy efficiency in compact applications.
The TMCM-1690-TMCL is a single-axis field-oriented control (FOC) servo controller gate driver module for 3-phase BLDC and DC motors. Universal asynchronous receiver-transmitter (UART) and controller area network (CAN) interfaces enable TMCL protocol support for communication. Position feedback can be supplied via incremental encoders, digital hall sensors, and absolute SPI encoders.
The TMC5240 motion controller and driver chip is an intelligent power component designed to interface between a CPU and a stepper motor. All stepper motor logic is completely within the TMC5240 with no software requirements. The TMC5240 offers numerous unique enhancements, which are enabled by the system-on-chip integration of the driver and controller. Typical applications include 3D printers, lab and factory automation, antenna positioning, and more.
To read the new eBook, visit https://analog.mouser.com/adi-ebooks/14-experts-discuss-motor-control-in-modern-applications/. To view more eBooks created by Mouser and ADI, visit https://analog.mouser.com/adi-ebooks/.
To browse Mouser's entire manufacturer eBook library, visit https://resources.mouser.com/manufacturer-ebooks/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.