Mouser Electronics and Analog Devices Present Webinar on Advancing Industrial Automation with Smart Sensor Solutions

För omedelbar lansering

Anslut till oss


8 April 2025Mouser Electronics, Inc., the authorised global distributor with the newest semiconductors and electronic components, has partnered with Analog Devices, Inc. (ADI) to provide the engineering community with a new webinar titled “Engineering Reliable Industrial Automation with Sensor Fusion”. This free-of-charge webinar will take place on 29th April 2025 at 17:00 CET.

Industrial automation is pivotal in driving operational efficiency and precision across a wide number of sectors, including manufacturing, distribution, heavy industry, and construction. However, the performance of these complex automation systems relies on high-quality sensing technologies. These reliable, high-accuracy sensors are needed to enable the continuous real-time monitoring of critical parameters like pressure, temperature, flow, and position sensing.

For engineers, the seamless integration of diverse sensing technologies is needed to create fast and reliable industrial automation solutions that minimise downtime and maximise consistency and precision. This webinar will provide actionable insights into the latest sensing technologies and best practices for designing robust industrial automation systems.

By attending this webinar, participants will learn more about:

  • How sensors are utilised in industrial automation to monitor system health and predict potential component failure.
  • The factors that contribute to the success or failure of seemingly similar inertial sensors in meeting the demands of the upcoming robotics revolution.
  • The methods to eliminate the need for re-homing industrial automation equipment.
  • Innovative products from ADI that help to enhance industrial automation accuracy and reliability, including:
    • ADMT4000 True Power-On Multi-Turn Position Sensor, which is a magnetic position sensor capable of recording the number of rotations of a system even while the device is powered down.
    • ADXL380 3-Axis MEMS Accelerometers, which are low-noise, low-power 3-axis MEMS accelerometers that incorporate a built-in micropower temperature sensor, multi tap detection modes, and a state machine to prevent false triggering.
    • ADIS1657x Precision MEMS IMU Modules, which are precise MEMS inertia measurement units (IMUs) featuring a triaxial gyroscope and accelerometer with signal conditioning, SPI data communication, and robust shock survivability.

The webinar will be hosted by Mark Patrick, Technical Content Director, Mouser Electronics in EMEA and will feature Enda Nicholl, Strategic Marketing Manager for Magnetic Sensors, ADI and Tzeno Galchev, Director, Marketing and Applications for Inertial Sensors, ADI, as guest speakers.

To watch the webinar live or to receive a recording of the webinar when it becomes available, sign up at https://emea.info.mouser.com/webinar-adi-industrialsensors-emea/.

To learn more about ADI, visit https://www.mouser.com/manufacturer/analog-devices/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För pressförfrågningar, kontakta:
Janice Fenton
Direktör för B2B-kundansvar med ansvar för originalitetsverifiering
+44 (0) 7984 077330
För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833