ADAS: The Key to Reaching Level-5 Autonomous Vehicles
June 1, 2021 - No longer relegated to science fiction and fantasy, fully autonomous Level-5 vehicles — free from geofencing and capable of going anywhere and doing anything that an experienced human driver can do — may integrate onto our roadways within the next 10 or 20 years. According to the U.S. National Highway Traffic Safety Administration (NHTSA), the primary benefit of vehicle automation will be added vehicle safety. As the technology evolves and automakers progress through the six automation levels on the road to full automation, advanced driver assistance systems (ADAS) are leading the way by providing and delivering an overall better vehicle driving experience.
Level-5 autonomous vehicles (AVs) will likely be electric vehicles (EV) with robust, onboard, fully connected vehicle-to-everything (V2X) communication systems. For these Level-5 AVs to function as envisioned, they will need to be able to seamlessly communicate with other vehicles on the road while simultaneously monitoring the road environment, self-diagnosing their onboard electrical systems, and identifying every potential road hazard — all while keeping passengers safe and comfortable.
Although this futurist outlook of fully autonomous Level-5 EVs is exciting, the reality according to most automotive experts is that this level of vehicle autonomy is still years maybe even decades away. Most of today's new vehicles have Level-1 autonomy integration features, such as Adaptive Cruise Control (ACC) and Lane Keep Assist (LKA) to help with driving fatigue and nudge drivers back into the lane should they veer off a bit.
Automakers are fast-tracking their efforts into integrating Level-1 systems into true Level-2 ADAS. In Level 2, AVs let the ADAS systems assist with braking and steering functions but still require the driver to be in control and monitor the vehicle's environment, especially in safety-critical situations. The next most significant jump to Level 3 will still require the driver's attention, but that level of automation will allow the vehicle to fully perform safety-critical functions like braking without any significant intervention from the driver through advanced sensor systems like cameras, radar, and light detection and ranging (lidar).
Mouser Electronics partners with dozens of leading manufactures that are innovating in this ADAS and AV space. Together with these manufacturers, Mouser provides relevant and engaging content, such as eBooks on smart mobility technologies and connectivity solutions and application-focused resource sites, to put engineers at the forefront of automotive technology. Engineers can keep up with the latest trends and technologies by subscribing to Mouser's customized newsletters and following the award-winning Empowering Innovation Together™ program.
To further stay on the leading edge, engineers need genuine components for their designs. Buying from an authorized distributor is the only way to eliminate the risk of counterfeit or gray market products. Mouser customers can order with confidence, knowing that the global authorized distributor has rigorous processes in place to prevent counterfeit products from entering its inventory. Mouser has received accreditation to AS6496, AS9100D, ISO 9001:2015, and ANSI/ESD S20.20-2014, the industry's gold standards for quality, control, and electrostatic discharge (ESD). Over 1,100 semiconductor and electronic component manufacturer brands count on Mouser to help them introduce their products into the global marketplace. Customers can expect 100% certified, genuine products that are fully traceable to each manufacturer.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.