Mouser Long-Term Partner DS PENSKE Formula E Team Racing Team Heads to Italy's Adriatic Coast for Misano Doubleheader

För omedelbar lansering

Anslut till oss


Learn more about the Mouser-backed DS PENSKE Formula E racing team
Photo: DPPI

April 9, 2023Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is ready to cheer on the DS PENSKE Formula E racing team in Misano, Italy, for rounds 6 and 7 of Season 10 of the ABB FIA Formula E World Championship. The race weekend will kick off on April 13 for round 6 and continue on April 14 for round 7.

The races are taking place at the iconic Misano World Circuit Marco Simoncelli circuit, which is located in the beautiful Emilia-Romagna region. Usually home to Grand Prix Motorcycle (MotoGP) and Superbike World (WorldSBK) racing, as well as endurance and sports car racing, the circuit was designed in 1969 before opening in 1972. For Formula E's first visit, the circuit will run to 3.382 km with 14 turns. It's a rapid, flowing track with plenty of overtaking opportunities and room for maneuvers. The DS PENSKE Racing team has two past Formula E Champions driving its cars, 2022 World Champion Stoffel Vandoorne and the unique two-time Formula E Champion, Jean-Éric Vergne.

Mouser is supporting the DS PENSKE team for the globe-trekking 2024 season in collaboration with TTI, Inc. and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.

The Formula E series features cars that are powered solely by electricity and represent a vision for the future of the motorsports industry, serving as a framework for research and development around zero-emission motoring. Using the very latest technology, the DS Performance Development Team has stretched the boundaries of efficiency and performance with the DS E-TENSE-FE23 powertrain and software. Racing is all about speed and endurance, and racing sponsorships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

To learn more about the Mouser-backed DS PENSKE Formula E team and view the 2024 Formula E schedule, visit https://www.mouser.com/formula-e/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764