Mouser-Sponsored Formula E Racing Team Readies for Berlin Doubleheader on Updated Track

För omedelbar lansering

Anslut till oss


Learn more about the Mouser-backed DS PENSKE Formula E racing team
Photo: DPPI

May 7, 2024 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is ready to cheer on the DS PENSKE Formula E racing team in Berlin, Germany, for rounds 9 and 10 of the Season 10 ABB FIA Formula E World Championship. The race weekend will kick off on May 11 for round 9 and May 12 for round 10.

The DS PENSKE team is coming off a strong showing at the Monaco E-Prix, where 2022 World Champion Stoffel Vandoorne claimed third place and two-time Formula E Champion Jean-Éric Vergne secured a very close fourth-place finish. The Berlin races will again be taking place at the historic Tempelhof Airport, where the track has been given a fresh makeover, incorporating longer straights and technical sections into a speedy track layout. A major characteristic of the Tempelhof Airport circuit is its abrasive track surface, which is made up of repeating concrete slabs. As a result, drivers have to nurse their tires along the track surface, making for an even tougher test against the speed and the of the track. The new circuit aims to favor the current Gen3 cars, which have proven to be faster, lighter, and more efficient compared to the previous Gen2 cars, with a 2.585 km (1.6 mi) long layout. The Gen3 cars can flex their immense speed along the straights, while the hairpins provide a great opportunity to make an overtake.

The Berlin Formula E weekend will also include a Rookie Test race, with Jonny Edgar and Robert Shwartzman driving for DS PENSKE. Edgar previously raced in the FIA Formula 3 Championship, taking victory in the season finale in Monza. Shwartzman is a reserve driver for the Scuderia Ferrari Formula 1 team.

Mouser is supporting the DS PENSKE team for the globe-trekking 2024 season in collaboration with TTI, Inc. and valued manufacturers Molex and KYOCERA AVX. Mouser and Molex have been partnering to sponsor Formula E racing since 2015.

Formula E is an international, fully electric street racing series. Using the very latest technology, the DS Performance Team has stretched the boundaries of efficiency and performance with the DS E-TENSE-FE23 powertrain and software. Racing is all about speed and endurance, and racing sponsorships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.

To learn more about the Mouser-backed DS PENSKE Formula E team and view the 2024 Formula E schedule, visit https://www.mouser.com/formula-e/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764