Mouser Explores the Challenges of Powering AI in New Interactive eBook from Renesas Electronics

För omedelbar lansering

Anslut till oss


Read the new interactive eBook from Renesas
Read the new interactive eBook from Renesas

February 3, 2026Mouser Eklectronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announces a new Interactive eBook in collaboration with Renesas Electronics that explores how data centers are evolving to meet the power demands of artificial intelligence (AI).

The requirements of Generative Artificial Intelligence (GenAI) are pushing data center power consumption ever higher. The cost of running a data center was already heavily driven by its electricity bill, so this surge in consumption has only led to an increased importance in energy efficiency for data center power management. In Powering AI: High-Density Power Distribution in Modern Data Centers, AI industry-leading experts discuss topics such as the shift to higher-voltage power delivery and how digital power technologies enhance energy efficiency. Videos demonstrate how liquid cooling enables higher server density and how utilizing more efficient gallium nitride (GaN) and metal-oxide semiconductor field-effect transistors (MOSFETs) in power circuits allows engineers to design smaller, lighter power systems. The eBook also includes an interactive infographic detailing how power flows through a typical data center. Renesas has a long history in the field of power management and offers customers a broad portfolio of products and solutions, many of which are highlighted in the eBook. Among the Renesas products available from Mouser are:

The Renesas REXFET-1 power MOSFETs feature ultra-compact, leadless designs for enhanced thermal performance, management, and reliability. The REXFET-1 wafer manufacturing process enables the devices to reduce on-resistance by up to 30 percent and an up to 10-percent reduction in Qg characteristics for higher efficiency.

The ISL99390FRZ smart power stage (SPS) module offers best-in-class current sense accuracy over line, load, and temperature. When combined with a Renesas digital PWM controller, these devices enable precision system-level power management and best-in-class transient response for loadline-based regulators. These devices simplify design by eliminating typical DC resistance (DCR) sensing networks and associated thermal compensation components.

The ISL68239 12-phase PWM controller uses the proprietary Renesas digital synthetic current modulation scheme to achieve the industry-best combination of transient response, ease of tuning, and efficiency across the full load range. Developers can use the intuitive Renesas PowerNavigator™ software to easily configure and monitor the device.

The TP65H015G5WS SuperGaN® FET combines a state-of-the-art high voltage GaN HEMT with a low voltage silicon MOSFET to offer superior reliability and performance. The device uses advanced epitaxy (epi) and patented design technologies to simplify manufacturability while improving efficiency over silicon via lower gate charge, output capacitance, crossover loss, and reverse recovery charge.

To read the new interactive eBook, visit https://www.mouser.com/renesas-powering-ai-ebook/. To browse Mouser's entire manufacturer eBook library, visit https://resources.mouser.com/manufacturer-ebooks/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764