Mouser Electronics and Hartland Controls Announce Global Distribution Agreement
December 6, 2021 – Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, announces a global distribution agreement with Hartland Controls, a Littelfuse company and supplier of components used in HVAC and other industrial applications. According to the agreement, Mouser will offer customers a range of motor run capacitors, definite purpose contactors, transformers, and other electrical control solutions.
“We are excited to collaborate with Mouser to distribute our electrical control devices for the HVAC industry worldwide,” said John Collins, vice president industrial controls and sensors at Littelfuse. “Through their logistics expertise and renowned customer service, Mouser helps to empower innovation and move our industry forward. We look forward to mutual success.”
“HVAC solutions and other industrial applications require a broad range of mission-critical components, and Hartland Controls consistently delivers reliable performance with impressive service life,” said Andy Kerr, Vice President of Supplier Management at Mouser Electronics. “This distribution agreement gives engineers around the globe an expanded choice of Littelfuse products when designing the next generation of electrical control solutions.”
The Hartland Controls HCK motor run capacitors boost the current or reduce the power factor to an electrical motor, delivering reliable power supply for a range of applications, including HVAC, food and beverage, electronics, and pools and spas. The start capacitors offer 370 VAC and 440 VAC rated voltage as standard, with 0.1% maximum dissipation factor and 30 µA maximum leakage current.
HCT 40 VA, 50 VA, and 75 VA transformers efficiently change one AC voltage to another by magnetic induction. The 40 VA and 5 0VA transformers are inherently limited, requiring no secondary fusing, while the 75 VA transformers are not inherently limited and do require secondary fusing. The transformers are ideal for applications such as food service, water pumps, and HVAC.
The HCD series three-pole definite-purpose contactors use three wires to control electrical current direction and are typically used in commercial applications. The contactors are rated for 50 FLA to 120 FLA and feature a +130°C Class B insulation system.
HCC series devices are also three-pole definite-purpose contactors, rated for 50 FLA to 60 FLA. The contactors feature a Double E magnet assembly for optimal performance with reduced power use, in addition to an actuator molded from high arc-resistant polyester. The contactors offer reliable performance for commercial and residential HVAC, water and wastewater, and electric vehicle (EV) charging.
To learn more about Hartland Controls products available from Mouser, visit https://www.mouser.com/manufacturer/hartland-controls/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
2026 - Hartland Controls, a Littelfuse company, is a supplier of electrical components used primarily in heating, ventilation, air conditioning, refrigeration (HVAC/R), and other industrial applications. This company specializes in the manufacturing and design of mission critical electrical contactors, class II transformers, capacitors, relays, auxiliary switches, and configured assemblies.
Om Littelfuse
2026 - Littelfuse (NASDAQ: LFUS) är ett företag som tillverkar industriteknik för en hållbar, uppkopplad och säkrare värld. I mer än 15 länder och med 17 000 medarbetare världen över, samarbetar vi med kunder för att designa och leverera innovativa, pålitliga lösningar. Våra produkter betjänar över 100 000 slutkunder och finns på en mängd olika slutmarknader inom industri, transport och elektronik – överallt, varje dag.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.