Mouser Electronics Headquarters Receives a Visit from the HARTING Roadshow Truck

För omedelbar lansering

Anslut till oss


February 13, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, and its employees received a special visit last week by the HARTING Truck, a traveling technology roadshow spotlighting the latest innovations from HARTING, one of Mouser's valued manufacturer partners. The HARTING Truck visited the Mouser headquarters in Mansfield, Texas, on February 4 to showcase their newest products.

The HARTING Roadshow Truck is loaded with displays of HARTING products, everything from heavy-duty industrial connectors to board-level solutions to market-leading IoT and RF technology. Complimenting each product station is a touchscreen app with data sheets, white papers, and videos. Mouser employees could take a break and enjoy a refreshment while chatting with HARTING's engineers to learn about their newest products.

"Events like this are a great opportunity for our team members that don't get to go to the big conventions and expos to interface with one of our valued manufacturers," said Eric Wendt, Mouser Vice President of Supplier Management. "The HARTING Roadshow gives our employees a chance to talk directly to the experts on these products and learn how their solutions can solve our mutual customers' needs."

Since 2003, Mouser has offered HARTING's extensive portfolio of over 23,000 high-quality electrical connector solutions for use in mechanical and plant engineering, broadcast and entertainment, factory automation, power generation and distribution, as well as industrial electronics and telecommunication. Mouser currently has over 7,000 HARTING part numbers in stock and ready to ship, including the HAN® ORV3 heavy-duty power connectors. The HAN ORV3 connectors are ideal for data centers and OCP spec power shelves.

The M17 circular connectors, available from Mouser, offer IP66/IP67 protection ratings, a 3.5mm to 13mm cable clamping area, and >500 mating cycles. These connectors are suitable for assembly stations, conveyor belts, packaging machines, industrial robots, and motion drive systems.

HARTING's SPE M12 T1 switches allow up to seven single-pair Ethernet (SPE) end devices to be connected to applications such as machinery, railway, robotics, and industrial automation. This design allows engineers to easily integrate sub-networks with SPE devices in their applications. These switches feature robust metal housing, an M12 interface, an IP65/IP67 protection rating, and PushPull locking that reduces errors and downtime.

To learn more about HARTING products, visit https://www.mouser.com/manufacturer/harting/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About HARTING

2026 - HARTING is the gold standard in connectivity for industrial environments and mission-critical applications.   As the pioneer in connectivity, HARTING combines the quality and customer service of its family-owned operations with a global footprint backed by in-region manufacturing facilities and local teams with deep engineering expertise.

With a reliable and robust approach to connectivity for any environment, HARTING enables improved efficiency and sustainability and future-proofs the businesses of today to power the innovations of tomorrow.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764