Mouser's Empowering Innovation Together Technology Installment Brings Engineers Up to Speed on WiFi7

Unlock the Benefits of WiFi7 with Expert Insights and In-depth Discussion
För omedelbar lansering

Anslut till oss


November 2, 2023Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, unveils its latest installment of the award-winning Empowering Innovation Together (EIT) technology series today, examining WiFi7 and the ways it will revolutionize wireless communication. WiFi7 will usher in a new era of wireless technology and pave the way for faster, more reliable connections.

Key specifications of WiFi7 include advanced features like quadrature amplitude modulation (QAM), automated frequency coordination (AFC) and multi-user multiple inputs and multiple outputs (MU-MIMO), which will significantly increase the speed, capacity and reliability of current wireless networks. WiFi7 promises to reconstruct the way we connect with others by providing faster and more reliable access to data, streaming services and online gaming experiences than ever before. Mouser sheds light on the technology behind this innovative wireless technology throughout the EIT technical content series, including articles, video and its signature podcast, The Tech Between Us.

"The anticipation for WiFi7 is real – with its promise of faster internet speed, stronger network connections and a more adaptive experience. Our EIT technology series is designed to give engineers the knowledge they need to stay ahead of emerging trends," says Mark Patrick, Mouser Electronics Director of Technical Content in EMEA, and the guest host of The Tech Between Us. "WiFi7 offers an incredible leap forward in wireless technology, and we are excited to offer a comprehensive  look at how this  technology will impact the world around us."

Through a range of articles, infographics, videos and The Tech Between Us podcast, Mouser offers valuable insight to the design engineering community on the advantages associated with this new technology, such as improved performance, additional security features, immersive technology capabilities, 8K streaming video and the relationship between WiFi7and 5G. The content notes how to leverage this cutting-edge technology in a wide variety of applications.

This EIT installment is sponsored by Mouser's valued partners Intel, Broadcom, TE Connectivity, Taoglas, u-blox, Qorvo, TDK, and KYOCERA AVX.

Established in 2015, Mouser's Empowering Innovation Together program is one of the industry's most recognized electronic component programs. To learn more, visit https://www.mouser.com/empowering-innovation/ and follow Mouser on Facebook, LinkedIn, Twitter, and YouTube.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764