Arduino MKR WAN 1300 and MKR GSM 1400, Now at Mouser Electronics, Offer Low-Power Connectivity for IoT Edge Devices

Nya produktlanseringar

Anslut till oss


Arduino MKR WAN 1300 and MKR GSM 1400, Now at Mouser Electronics, Offer Low-Power Connectivity for I

April 2, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the MKR WAN 1300 and MKR GSM 1400 from Arduino.

The Arduino MKR WAN 1300 and MKR GSM 1400 boards are designed to offer a practical and cost-effective solution for developers, makers and enterprises, enabling them to quickly add connectivity to their projects and ease the development of battery-powered Internet of Things (IoT) edge applications. Offering 32-bit computational power similar to the Arduino MKR ZERO board, both the MKR WAN 1300 board and MKR GSM 1400 board are based on a Microchip SAM D21 microcontroller, which integrates an Arm Cortex-M0+ processor, 256 Kbytes of flash, and 32 Kbytes of SRAM.

The MKR WAN 1300 board adds LoRa connectivity through a Murata CMWX1ZZABZ Lo-Ra module and can be powered using two 1.5V AA or AAA batteries, or from an external 5V supply. The MKR GSM 1400 board adds a GSM module for global 3G communication and provides a rich set of Input and output (IO) interfaces, including eight digital IOs; 12 PWM outputs; UART, SPI and I2C interfaces; analog IO including seven inputs and one output; and eight external interrupt pins.

Both of the highly compact boards measure just 67.64 x 25.00 mm and offer low power consumption, making them an ideal choice for emerging battery-powered IoT edge devices in the MKR form factor for applications such as environmental monitoring, tracking, agriculture, energy monitoring and home automation.

To learn more about the MKR WAN 1300 board, go to www.mouser.com/arduino-mkr-wan-1300. For more information about the MKR GSM 1400 board, visit www.mouser.com/arduino-mkr-gsm-1400.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About Arduino

2026 - Arduino is the leading open-source hardware and software company in the world. Born to provide an easy-to-use platform for anyone making interactive projects, Arduino has reached a growing community and adapted to new needs and challenges, branching out into products for IoT, wearables, 3D printing, and embedded environments. As of today, the Arduino community includes over 33 million estimated active users. With the Pro range, Arduino supports companies that are interested in going beyond the concept and rapid prototyping phase, to start mass production with the support of a qualified industrial partner and high-performance technological solutions.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764